Part Number: TIDA-010242 Other Parts Discussed in Thread: LM5069 , LM7480 Hi,
My question relates MIL-STD-1275E Surge Protection Reference Design which using L M74800DRRRQ1 and LM5069MM-2 devices:
In the Design Guide TIDA-010242 is written "the output of the…
Part Number: TIDA-010242
To whom it may concern,
I'm trying to understand the behavior of the TIDA-010242 reference design during the -250V spike. During the -250V spike, the TVS diode will clamp the voltage to a negative clamping voltage so how it…
Part Number: TIDA-010242 Good Morning,
I am working through the apps note for the TIDA-010242 and checking the calculations with a view to modifying or creating a similar design for a slightly modified version of 1275D.
I am currently looking at the SOA…
Part Number: TIDA-010242 Hi,
Is there any excel calculator for mosfet selection etc.for higher current systems which are 10A or higher. Because our system operate at 20A
Part Number: TIDA-010242 Thanks for a nice app. note.
Can you elaborate on the purpose and/or critical parameters of the capacitor C7, which is connected between GND and the middle point of the TVS diodes D3+D5.
C7 can be found on the schematics: https…
Part Number: TIDA-010242 Other Parts Discussed in Thread: LM5069 I plan to use this reference circuit in our product but I'd ideally like an input/output range 7-36V, the current schematic states 23-33V
I plan to increase D4 slightly to achieve the…
Part Number: TIDA-010242 To whom it may concern,
I have the following question about the TIDA-010242 MIL-STD-1275E reference design:
I am traying to understand how does the TIDA-010242 circuit work and I would like to customize it for my application…
Part Number: TIDA-010242 Other Parts Discussed in Thread: LM5069 , LM7480 Hi;
About the TIDA-010242 MIL-STD-1275 referance design curcuit;
I am traying to understand how does curcuit work for normal operation.
I am consederating to use this curcuit into…
Part Number: ESDS311 Other Parts Discussed in Thread: TIDA-010242 Hi All,
How many levels of IEC61000-4-5 has been tested for ESDS311? Please tell me the level of IEC61000-4-5.
Also, are there any other surge protection diode arrays that can provide MIL…