Part Number: TIDA-010265 As a Hardware design engineer how I can give the instructions to SW developer for motor controller to sense the ADC voltage of each phase coming from opamp and develop SW
1.what should be the delay b/w swithcing the each pin…
Part Number: TIDA-010265 Other Parts Discussed in Thread: TIEVM-MTR-HVINV Tool/software: hello,
I am testing the "TIEVM-MTR-HVINV 750W High-Voltage Motor Inverter Evaluation Module", but there are some problems. when I build the level 1 to test, there…
Part Number: TIDA-010265 Other Parts Discussed in Thread: TIDM-02010 , Tool/software: Hello,
I would like to understand the significance of below motor parameters and how does it impacts motor operation
USER_MOTOR1_FLUX_EXC_FREQ_Hz
USER_MOTOR1_FREQ_NEARZEROLIMIT_Hz…
Part Number: TIDA-010265 Tool/software: Is it possibe use the reference design to control a iii phase induction motor whit this hardware ?
if yes what are the steps to do the control program
Part Number: TIDA-010265 Tool/software: Dear support team,
I recently discovered that MOTOR_CONTROL_SDK is now 5_02 and include TIDA-010265 example with new features:
"Updated TIDA-010265: Updated design showing integration of IEC60730 compliant SDL…
Part Number: TIDA-010265 Tool/software: 1.Fast recognition, after MOTOR_ALLIGNMEN state, only one MOTOR_OL_START is executed, and then directly into the speed closed-loop (MOTOR_CTRL_RUNNING/MOTOR_CTRL_RUN), low-speed Iq will jitter, how can I actually…
Part Number: TMS320F2800132 Other Parts Discussed in Thread: TIDA-010265 , Hi Team
I try to download the project of TIDA-010265, but it report the issue: Break at address "0x3fff08" with no debug information available, or outside of program code.
…
Part Number: TIDA-010265 Hi team,
I'd like to build board based on TIDA-010265, but some part number from Wurth Elektronik seems to be garbled. Would you please share correct part number for C34, C38, C39, C42 and Y1?
Best regards,
Kuru…
Other Parts Discussed in Thread: TIDA-010265 , TIDM-02010 Hi,
We recently participated in Webinar: HVAC Heat Pump Motor Drives by Chris Clearman
We would like to evaluate the TIDA-010265 : which is single motor reference design. We could get the TIDM…