Part Number: TINA-TI Other Parts Discussed in Thread: TIDA-01040 , OPA827 , INA128 Hello,
I am trying to do transient analysis with TINA-TI and keep getting the error "Convergence problem. Check the analysis parameters!"
What can I do to solve…
Hello Kailyn,
Here's a couple of examples you can refer to for the input stage:
https://www.ti.com/lit/ug/tiduby8b/tiduby8b.pdf Check the non-isolated inputs
https://www.ti.com/lit/ug/tiduby7a/tiduby7a.pdf Its very similar to the above one
https:/…
Hi Ludovic,
The ESR resistor can vary from design to design. The recommended ESR on the output capacitor is from 1 Ω to 1.5 Ω.
In the design below:
www.ti.com/.../TIDA-01040
The ESR resistor they use is:
R134 1.00 RES, 1.00, 1%, 0.1 W, AEC-Q200 Grade…
Hi user,
Thank you for considering the LM5170. Two main reasons behind the 3V recommendation: (1) to avoid ending up with a too high current for the targeted 48V-12V power train application, which is usually above kW; and (2) there is a RAMP min voltage…
Other Parts Discussed in Thread: INA148 , INA149 How do Instrumentation Amplifiers (IAs) fit into my design?
TI Precision Labs - IA
Introduction to instrumentation amplifiers Training Video
When to use an instrumentation amplifier Training Video
Instrumentation…