Part Number: TIDA-01088 Other Parts Discussed in Thread: MSP-FET Tool/software: TI C/C++ Compiler I'm following the TIDA-01088 reference design, for JTAG programming I'm using a Xilinx JTAG to USB cable from the board to my PC. The cable is accurately…
Part Number: TIDA-01088 Tool/software: TI C/C++ Compiler I'm working on the reference design TIDA-01088. I wanted to know if there's a way to develop a simulation of the working model before developing the actual meter?
Regards,
Hira
Part Number: MSP430F67641 Other Parts Discussed in Thread: TIDA-01088 , EVM430-F6779 Dears
We need a power calculation chip for the meter to detect the power consumption of the 220V AC input port. I found the TIDA-01088 solution, please help to determine…
Part Number: TM4C1294NCPDT Other Parts Discussed in Thread: TIDA-01088 Hi
I am attempting to use the ADC to capture the stepped down voltage waveform parameters of our local AC Supply.
On the scope, it is a 50Hz +/- 1V sine wave at the ADC pin.
Wondering…
Part Number: TIDM-THREEPHASEMETER-F67641 Other Parts Discussed in Thread: MSP430F67641 , TIDA-00601 , TIDA-01094 , TIDA-01088 Hi,
I am looking to confirm if the above part works with a non invasive CT sensor as well as the invasive system.?
ALL,
Is there any plan or solution to implement SD24 or Sigma-delta modulation in the MSP432P4111?
For the future utility meter needs iso-AD conversion solution, I believe as below:
http://www.ti.com/tool/TIDA-01088
Kyt
Hi Vijay,
Assuming you are referencing the TIDA-00601 or TIDA-01088 then you will know that these use the SN6501 transformer driver with a DA2304-AL transformer that has a 1:2.2 turn ratio. This should be maintained to keep the default MSP430F67641…
Hello Saurabh,
The MSP430F6747A is an upgrade from the MSP430F6736A so you should be able to port the EVM430-F6736/TIDM-SINGLEPHASEMETER resources quite easily. You can also refer to TIDA-01094/TIDA-01088 (three phase solution) for resources from your…
Part Number: MSP430F67641 Other Parts Discussed in Thread: MSP-FET Tool/software: TI C/C++ Compiler Hey,
I'm following the TIDA-01088 reference design, however the design guide gives little information regarding how to download the F67641 project to…