Part Number: TIDA-010938
Hello Ti team,
We are currently reviewing the TIDA‑010938 reference design and would appreciate your support in clarifying some details related to the PFC implementation , which are not explicitly covered in the available…
Part Number: TIDA-010938 Can I get a copy of the TIDA-010938 REV E2 BOM in Excel format? The only one on the site is a PDF. There is also a version of the BOM mentioned in an earlier forum post but it appears to be an older version with significant differences…
Part Number: TIDA-010938 Other Parts Discussed in Thread: TIDA-010933 , Hi,
I am planning to design a 10kW single-phase inverter powered from a 48V nominal LFP battery system with an operating input voltage range of 42V to 60V DC.
I would appreciate…
Part Number: TIDA-010938 Hello
I like to buy the develoment board for TIDA-010938 , If available can you please point us
where can we order the develoment board?
how can we get the firmware for this deveopment board ?
Thanks
Geb
Part Number: TIDA-010938 We are testing the GTI system in Lab 8 using the string inverter software. I have noticed that the PWM signal is not syncing with the mains. Please provide a solution for checking the zero-cross in software, and which function…
Part Number: TIDA-010938 Tool/software: Hi, I would like to know if there are any simulation files for this product, and if so, can you tell me where they are located?
Part Number: TIDA-010938 Tool/software: Hi,
I noticed that the on-resistance of the GaN device is 30 milliohms, would it be feasible to replace it with a 70 milliohms product instead
Part Number: TIDA-010938 Tool/software:
in the design program file run lab 1 but if not "(stringINV_clearPWMTripBoost == 1U) " not show open loop and closed loop PWM in any LAB so, these variables not set in any placed so its reset or set to 1, and…