Part Number: TIDA-01333 Other Parts Discussed in Thread: TVS2700
Hello TI Support,
I was reviewing TIDA-01333 front end, and got the following questions
#1 What is the maximum VIN rated for (continuous)? #2 How is the input protected against…
Part Number: TIDA-01333 Other Parts Discussed in Thread: ISOW7841 , TPS55010 , , INA149 Team,
If ISOW7841 provides isolated power, why does this reference design use TPS55010?
Thanks
Viktorija
Hi Lars, thank you for your detailed reply, I found this reference design TIDA-01333 ( www.ti.com/.../TIDA-01333 ) which I think should be more suitable for my application. I just have 2 questions: Firstly, is it possible to implement the open wire detection…
Other Parts Discussed in Thread: TIDA-01333 , TIDA-00764 , TIDA-00170 , ADS8688A , TIDA-010008 , ADS8694 , ADS8684 , ADS8688 , ADS125H02 , MUX36D04 , MUX509 , UCC12040 , SN6505B , UCC12050 Hi
We are designing Analog input module for following requirements…
Other Parts Discussed in Thread: TIDA-01333 in the data sheet appears the section with the following text "and each channel can be configured as a current or voltage input with software configuration" i have a 4-20 ma sensor , how to configure current…
Hello Zeeshan
Need for group isolation will simplify the design.
The switch and the interface can be controlled using digital isolators.
Please refer the below and note that we may not have solutions exactly matching your requirement.
TIDA-00118…
Hello VEERAMANI,
Welcome to E2E forum.
It depends on if you need or want to isolate your data acquisition system with your backend processor system.
If no, please refer to ADS8681EVM which is a ADC in same family but doesn't have any digital isolator…
Hi Alessandro,
Thanks for your query on E2E. Absolutely you can use ADS8681 for 4-20mA signal acquisition. We have some released TI Designs that introduce the solution for voltage (Max. ±12.288 V) and current (0~24mA) signal based on ADS8681:
www…
1. front-end amplifier would be better choice
2. pull-down may case other problem
3. simulaneous-sampling is always needed, ADS8900B is my first choice, use ADS8691 just because it's simple, only one power need, if add front-end amplifier, additional…
Noam,
Thanks for clarifying your design intent, I wanted to make sure you were looking for an additional external MUX.
If you are looking to multiplex 4 differential analog inputs the MUX36D04 seems like a good device. This part is used in industrial…