Hi,
As your input voltage minimum is 8.5V compared to TIDA-01352 24V, the transformer turns ratio for TIDA-01352 Np:21Ns = 1:7.5, then yours should be Np:Ns = 1:(7.5 x 24/8.5) = 1: 21.2. Other parameters can be similar to TIDA-01352 transformer 750343547…
Other Parts Discussed in Thread: TIDA-01352 , LM5030 , TIDA-01592 , LM3481 , TIDA-010057 , LM3488 , LM3524D
I have referred following documents so please find my query/comments as under.
TIDA-01352
>> This board is based on LM5030 with push…
Part Number: TIDA-01592 Other Parts Discussed in Thread: TIDA-01352 , LM5030 Dir Sir,
For ultrasonic application. We survey a power solution that implements +-100V, such as TI solution TIDA-01592.
But power budget is not enough for this application…
Part Number: TIDA-01371 Other Parts Discussed in Thread: TIDA-01352 Hi,
The Peak power consumption formula in page 3 of the TIDA-01371 is shown below
Peak power consumption = 4 *128 *470p *100*100* 7.5M = 18 kW.
Q1. From where the multiplication…
Hi Jason,
Sorry for the delay in replying.
We have two TI Design for transmit power supply: TIDA-01352 and TIDA-01371. The TIDA-01352 is the SMPS for generating +/- voltage rails for the tranmit power supply. TIDA-01371 is floating regulator design…
Hi Scott,
Can I use the output stage of this reférence ( www.ti.com/.../TIDA-01352)design to get an output of 150 volts ?
If it's possible to use it, which IC can replace the lm5030 to allow me to drive the output with the tdc tx pin?
Hello Fukazawa,
With this limited information, I would suggest TIDA - 01352 is a good choice of a power supply with scalable output and high efficiency with LM5030 integrated.
Section 2.3.2 talks in great lengths about designing the push-pull power…