Hi Francisco,
There is programmer reference design for I2C TIDA-01373TIDA-01373 reference design | TI.com
The device can be Sleep or Standby, in case of I2C we need to maintain Speed Pin to know state (High / low) , please refer to the information…
Jay,
The EEPROM write cycle is 1000 for this device. The procedure in the datasheet shouldn't have any issues because we follow the same steps in our GUI and we could write to EEPROM. , I'd recommend referring to the code as a reference (Link: https…
Part Number: DRV10975 Other Parts Discussed in Thread: TIDA-01373 , We using of TIDA-01373 for writing DRV10975.
TIDA-01373 can supply 12v ~ 24v power.
And 22v or more is required to write the EEPROM of the DRV10.
However, DRV10975 has a Vinmax…
Hey Andy,
I am yet to go more in detail in your issue. However, I'd recommend referring to the code for this design as a reference http://www.ti.com/tool/TIDA-01373 . Look at the "TIDA-01373 DRV10983Q1_987 Example Code".
Sincerely,
Sanmesh U.
Let me get back to you on tuesday when my coworkers come back from holiday.
However, to write EEPROM, to my knowledge all you need is something that can communicate data through I2C.
TI provides the design files for the TIDA 01373 ( www.ti.com/.../TIDA…
Hello Jack,
I see you’re making an EEPROM programmer. We actually have a reference design that can program the EEPROM :
If you are not familiar, reference designs are designs that use various parts to enable an application. As a result, the designs…
Hi Ueli,
Is the customer interfacing their board with our DRV10983EVM & GUI? If so, can we confirm how they are doing it (wiring, process, etc)?
Have they looked at the DRV10983 gang programmer for strategies?
DRV10983EVM-TB can be used to write…
Part Number: MSP430FR5972 Other Parts Discussed in Thread: DRV10983 , TIDA-01373 Good Morning everybody!
Today I'm here because I noticed two different information in two related user guide for the same device and I really don't know what is the exact…
Hello Jonas,
I assume you're looking to program the EEPROM for a large amount of DRV10983 motor driver ICs. If so I would not recommend the USB2ANY and instead refer to our EEPROM Programming Tool Reference design (TIDA-01373). Generally speaking, the…
Programming is used to tune the driver to spin the motor. The only way ic can be used without programming is if the default ic settings can spin the motor.
Programming is done through I2C interface.
To enable easier programming, we provide the following…