Part Number: TIDA-01407 Sir,
We are using the TI reference deign TIDA 01407 for DC to DC converter in which facing the issue in 03nos of component which are use in this design.
Transformer, TH : Payton 59023 ( BOM serial number : 45)
Inductor…
Part Number: TIDA-01407 Other Parts Discussed in Thread: UCC27212A-Q1
Hello,
Mike as reply on the 16th Dec'21 for the TI design TIDA01407 for subject of " TIDA-01407: Issue observed in getting the output voltage" which was not generating the output…
Hello,
I reviewed your attached report.
1. Your input voltage is set at 30 V, and this is too low if you were using the TIDA-01407 that was designed for 36 to 60 V.
2. The waveforms in section 5 of your report show that the design is operating at…
Part Number: TIDA-01407 Dear All,
one of my customer interested to take TI design:
TIDA-01407 for 48V to 12V,30A application, they would like to complete details of transformer used in design - such as core, bobbin, winding informations - so they…
Part Number: UCC28951 Other Parts Discussed in Thread: TIDA-01407 , UCC27282 Tool/software: HI,
Thanks for reply my previous noise issue related to un-balance duty cycle of OUTC & OUTD.
I follow the UCC28951 IC parameter of " TI Designs: TIDA…
Part Number: UCC27531-Q1 Other Parts Discussed in Thread: UCC27301A-Q1 , UCC27311A-Q1 , TIDA-01407 , UCC27211A-Q1 , DRV8300-Q1 Hi Team,
I'd like to ask you about the high-side and low-side driver for 48V EV battery system. I couldn't find these devices…
Hi Rajesh,
Below are my responses to your query
rajesh Gudimani said: Is UCC28951 suitable for replacing ISL6754 in this application?
Yes, UCC28951 is functionally suitable as a replacement for ISL6754. Both are phase shifted full bridge (PSFB)…
Hello Shyama,
As you pointed out: In SLUA560C the RC of the secondary snubber is connected to the GND of the board and in TIDA-01407 the same in connected tot he Sec high. From an analog point of view, they both are AC grounds because there is no fluctuating…
There is more explanation of the design here: https://www.ti.com/tool/TIDA-01407
This may be the document you're interested in: https://www.ti.com/lit/ug/tiduda3/tiduda3.pdf