Hi Rock,
1. This is more of a data transformer question. If you select the data transformer or magjack rated for 10G, then it should be okay. Note PSE chip is independent of the ethernet data rate.
2. 10kv and 12kv surge as an extremely high requirement…
Hi Tommy, i looked through the excel sheet and the open items are all either system level software implementations or system level hardware implementations. For the TPS23861, from a software prospective, the product page has very simple reference code…
Hi Jamie,
1. If you are looking at the TPS23881EVM-008, this pairs with the MSP5969 launchpad and the TI.com reference code on the TI.com reference page. If you're looking at the TPS23881EVM-083 or FirmPSE reference design TIDA-050026, then it pairs with…
Part Number: TPS23730EVM-093 Other Parts Discussed in Thread: TIDA-01411 , TPS23730 Dear *,
1) i read that the CMC in Poe magnetic is recommended on cable side but in TPS23730EVM-093 magnetic used have CMC with three-wires on phy side.
1a) Why do you use…
Graeme, I suggest you start by reviewing our 6kV surge protection TI design for PSEs located here --> http://www.ti.com/tool/TIDA-01411 .
While it utilizes a different PSE (TPS23861 instead of the TPS23881), the methodologies and techniques utilized…
David,
I will answer question #1 and then pass this thread over to Penny (PSE Application Engineer) for #2.
1. How do I test whether the PSE equipment meets the POE specifications and performance?
There is a PoE interoperability test suite available…
Other Parts Discussed in Thread: TIDA-01411 The long-term industry prescriptive equipment safety standard IEC 60950-1 is due to be replaced by the hazard-based equipment safety standard IEC 62368-1 in about 2020. Currently there is IEC 62368-1 Edition…
Andy,
This topic is confusing and frustrating to many in the marketplace. In short, the answer is 'yes, with a footnote.' In my experience, I have not heard of a 'PoE+' solution having an interoperability issue with our TPS23861. As a matter of fact…