Part Number: TIDA-01485 Other Parts Discussed in Thread: DRV8323 , MSP430F5132 Hello,
I am trying to modify the reference design code such that the motor will freewheel (DRV8323 Sleep Mode), after the motor stops. Disable works after the initial run…
Part Number: TIDA-01485 Cap 2.3.1 pag 6 row 10.
There's a typo in ADC voltage input range calculation.
"Considering a 10% headroom for this value, the maximum recommended voltage input to the system is
25.3 × 0.9 = 42.5."
The correct value is…
Part Number: TIDA-01485 Other Parts Discussed in Thread: MSP430F5132 Hello,
This design uses P3.0 and P3.1 for UART communications, but I am not able to get it to work. I am able to get serial communications working using P1.1 and P1.2 for UARTutilizing…
Part Number: TIDA-01485 Other Parts Discussed in Thread: ENERGIA , MSP430F5132
Hello,
I had this PCB built for educational purposes, but I have not been able to get it to work. I have a few questions.
(1) SL_C is shown connected to C18 to the right…
Hello Manu,
Wow, thanks so much for the fast response and for linking the duplicate thread above. I will close this thread, since you've already provided guidance in the other thread.
Regards,
James
MSP Customer Applications
Part Number: CSD88599Q5DC Other Parts Discussed in Thread: TIDA-01485 Tool/software: Hello,
I’m evaluating the CSD88599Q5DC for a full H-bridge motor application (external driver), and I’d like to confirm if the MOSFET can handle the following operating…
Part Number: CSD88599Q5DC Other Parts Discussed in Thread: TIDA-01485 , CSD88584Q5DC , TIDA-00774 Tool/software: Dear TI,
I am puzzled by the datasheet information that why is the potential of the top "EXPOSED HEAT SLUG".
Do it connected to the…
Part Number: TIDA-010056 Hi,
I want to work on this reference design, also check others such as,
https://www.ti.com/tool/TIDA-00774
https://www.ti.com/tool/TIDA-01485
However, the gerber files in the zip cannot be extracted for some reasons…
Hi, Basit
There are TIDA as reference:
https://www.ti.com/tool/TIDA-010072
https://www.ti.com/tool/TIDA-01485
One of these is connect DRV with C2000.
Also, from MSPM0 side, we can connect DRV8323R.
But for MSPM0, we can only support 1 DRV8323…
Hi,
Please refer to TIDA-01485 too. ( www.ti.com.cn/.../TIDA-01485 )
But this is also the 6*PWM scheme. For the 1*PWM drive scheme, you can refer to TIDA-010031( https://www.ti.com.cn/tool/cn/TIDA-010031?keyMatch=TIDA-010031 ), which has 1*PWM code…