Part Number: TIDA-01494 Document No. : TIDUDF3
Page 7
I think there's something wrong in this page, In the inductance calculation formula it use 950000, but in the table, it should be 70k fsw
And the calculation result is also wrong, if you use 950000…
Part Number: TIDA-01494 Other Parts Discussed in Thread: UCC25600 in TIDA-0194 http://www.ti.com/tool/TIDA-01494
split capacitor LLC resonant converter is used , how to select the RMS voltage in this case.
Is it the same way what is mentioned in SLUP263…
Part Number: TIDA-01494 TIDA - 01494, this design support for output voltage 48VDC/15amp battery charging circuits.
What are the chances will be required to achieve the circuit design
Part Number: UCC256301 Other Parts Discussed in Thread: TIDA-01494 , How Can I get UCC256301 's transformer designing in TIDA-01494? It shown a part from WURTH.
Thanks!
Part Number: TIDA-01494 Other Parts Discussed in Thread: PMP20795 I want to check why TIDA-01494 have standby power on the EVM?
UCC2563X series IC is used for non-standby power design, right?
If customer want to test TIDA-01494 for non-standby power design…
Part Number: TIDA-01494 Other Parts Discussed in Thread: UCC28180 Hi!
Kindly explain what would be the purpose of the dual Comparator IC U1A whose output is connected to the FREQ pin of PFC Controller UCC28180. I do not understand the Concept behind …
Part Number: UCC256301 Other Parts Discussed in Thread: TIDA-01494 , , INA181 , UCC25600 Hello, While referring to TIDA-01494, I have some queries . Is the compensation network CC-CV charger for battery ? Could you share the calculator for calculating compensation…
Hey,
I want to built and evaluate the reference design TIDA 01494 does anyone know which heatsinks are used or a similar sample that can be used?
best regards
Michael
Part Number: TIDA-01494 Hi
We are looking for suitable Ti design for reference for 90~264 Vac in +/- 80Vdc 6A out solution. Any suggestion?
Thanks!
PY Tsai
Part Number: UCC256301 Other Parts Discussed in Thread: TIDA-01494 Hi Sir,
Form the document of TIDA-01494, it could dlivers 20A continuous current and up to 30A peak current for 3 seconds.
But the deley time of OCP3 level is only 50ms, how this design…