Part Number: TIDA-01495 Other Parts Discussed in Thread: UCC28063A Hello Ram sir ,
customer is planning to increase the maximum power rating of TIDA-01495 by an additional 100W .
Do you think the design and topology selected can still support .
Other Parts Discussed in Thread: TIDA-01495 Hi Everyone,
This TIDA-01495 model rated as universal power supply. But my doubt is what if need design to work in American standard like 110VAC whether the protection circuit like Fuse and MOV need to change…
Part Number: TIDA-01495 It looks like you are using a transformer as your boost inductors in the PFC circuit with the secondary providing feedback to the UCC28063DR. The BOM only lists this as a custom transformer and a value of 150uH but doesn't giver…
Part Number: TIDA-01495 Other Parts Discussed in Thread: UCC24612 I was wondering how the UCC24612 in the Synchronous Rectifier Driver section in the TIDA-01495 reference design gets it's power. It looks like VDD for both chips are connected to each other…
Part Number: TIDA-01495 I am designing a power supply based on this reference design and can't find Payton 58599. Is this a custom part form Payton? What are the necessary specifications for this component?
Part Number: TIDA-01495 There are a few inconsistancies with the documentation for this reference design. What were the final values used that made this design work? Specifically, what are the inductances and capacitances in the LLC circuit? What is the…
Part Number: TIDA-01495 How do you change/trim the output voltage? Am I understanding it correctly that I have to change the transformer ratio to make large voltage adjustments in the LLC circuit and then use R35 to make minor adjustments? Does that mean…
Part Number: TIDA-01495 Other Parts Discussed in Thread: TINA-TI , UCC28063 Tool/software: TINA-TI or Spice Models Hi,
I have attempted to import the UCC28063 Spice model into TINA-TI , and I got the following error.
Invalid device: $CDNENCSTART. Line: #40…
Hello Adam,
Thanks for posting this question.
Do you need 20A continuously/nominally or is that a peak requirement? (This will help clarify which topology is best suited for your power level)
If you're planning to use analog control, the following reference…