Hi Kevin,
Normally this would be a two stage design, a PFC stage + a dc/dc isolation stage.
For the PFC stage we would recommend the UCC28180 CCM PFC controller,
For the DC/DC isolation stage you can look at the UCC28951 phase shifted full bridge…
Yes we are still determining the best topology and control IC. Would a simple fixed current limit be easier? What happens to TIDA-01501 when the load impedance is too low? Is it not feasible to implement a current limit or one that is controllable? I…
Part Number: UCC25600 Other Parts Discussed in Thread: UCC29950 Hello,
While looking at the tool "sluc146,Rev 1.2 2009-04-29", the Peak_Gain(m) versus Qe plot in sluc146 is not the same as in SLUP263.
The plot in SLUP263, TIDA-01501 and TIDA-01557…
Hi Bo Xian Yeh,
TIDA-01557 is a PFC + LLC design without auxiliary: www.ti.com/.../TIDA-01557
PMP20795 is a LLC design without auxiliary supply (please note that this design is LLC only): www.ti.com/.../tidrsc3.pdf
TIDA-01494 and TIDA-01501 both…
Hi, Gary
UCC25600 is last generation LLC controller, there is new LLC controller is relased in TI, it is UCC25630.
please refer to below reference design, the solution is UCC28180+UCC25630.
www.ti.com/.../tida-01501
regards,
Yunsheng
Part Number: UCC256301 Other Parts Discussed in Thread: UCC29950 , Hi Sirs,
we have two 450W and 750W PSU project.
And we do reference TIDA-01501 for 450W project.
could this same chips solution apply to 750W?
or I saw UCC29950 can output 750W…
Dear Ben Lough,
thank you for your fast reply.
These are really nice features ...
But I am still confused about gate drivers. You mention low and medium power designs (do you consider about 500 W of the reference designs, TIDA-01501 or TIDA-01494…