Part Number: TIDA-010054 Other Parts Discussed in Thread: TIDA-01604 , TIDA-01605 Hi Team,
Why in TIDA-01604 is preferred to use TIDA-01605 instead of TIDA-010054?
in TIDA-010054, there is the part "Short circuit Detection & Two Level Turn Off For…
Part Number: TIDA-01604 Hi, support team
My customer has the questions as follow:
I have gone through TIDA-01604 design
1. Is it possible to design 7.2KW?
I need to convert 220vac, 50hz to 700vdc with nearly 8kw
2. If it is possible kindly…
Part Number: TIDA-01604 Other Parts Discussed in Thread: TIDM-02008
Hi,
We found this PFC Boost 6.6kW eval board in TI website, and we are intending to use it as the proof-of-concept of a product in McLaren Automotive. We need more information about…
Part Number: TIDA-01604 Hi team,
I'm reviewing TIDA-01604 and am curious why the Voltage loop ISR is running at 10kHz. This doesn't seem to be explained.
Could you help me understand:
Why the voltage loop is being run at 10kHz? It seems like overkill…
Part Number: TIDA-01604 Dear E2E team,
we are unable to get resource explorer online enable function.
Please guide us to make use of the option.
thanks
Bhima
Part Number: TIDA-01604 During the zero-crossing interval of my AC input voltage, I need to provide a blanking interval where both my EPWM1A and EPWM1B turns OFF i.e. goes low
Part Number: TIDA-01604 Hi,
I have a question regarding the Totem Pole PFC design.
we wish the PFC to dynamically “on the fly” change modes (PFC to inverter mode, and vice versa) with minimum delay (several milliseconds) utilizing bi-directional topology…
Part Number: TIDA-01604 Would anyone be able to share or point to few rule of thumbs to get a crude estimation of total board weight (PCB and components assembled) , empty unpopulated board, the components, and heat sinks?
Using the BOM PN# wherever…
Part Number: TIDA-01604 A square wave pulse of 50hz frequency is fed to gpio based on this input pwm pattern is generated which is shown below and code also is attached .the problem is at the rising and falling edge of pulse . how to rectify this problem…