Part Number: TIDA-01606 It seems that the duty cycle of SVPWM PFC and SVPWM inverter modes coincide, but how can I control its current direction or working mode?
Part Number: TIDA-01606 Dear TI Team
We have took TIDA-01606 as our reference for our 3-Phase GTI inverter
Now we are in the final stage of our testing and about to connect inverter with Grid
We would like to know what are the parameters need to be considered…
Part Number: TIDA-01606 Other Parts Discussed in Thread: ISO5852S , UCC21750 Dear TI,
Good morning.
In TIDA-01606,you can see IS05852S driver is being used to drive SiC MOSfet.
In ISO5852S driver in DESAT connection,along with 1000V RS1MWF-7 reverse voltage…
Part Number: TIDA-01606 Dear TI team,
Good morning.
We have sensing DC panel voltage in which we have used DC voltage sensing reference circuit from TIDA-01606.
Kindly find below details.
For example we are sensing DC panel voltage of 400V at no load…
Part Number: TIDA-01606 Hi Experts,
Good day.
Client is producing an inverter for compression for air condition and need to rebuild it.
It is THGA 5512C 400 – 440V/50 – 60Hz. Rated current RLA 1,7/1,8A Max. current 2,5/2,5A Start current LRA…
Part Number: TIDA-01606 Hello my friends, I'm trying to understand the software for TIDA-01606 bidirectional inverter/PFC but i have something that i didn't understand.
Why in the current loop they use Grid current instead of inverter current…
Part Number: TMS320F28379D Hi,
I want to design 3 phase grid tied inverter. I have seen this (TIDA - 01606) reference design.
1.65V is connected in 17th pin. 17th pin going to ADCINA3.
I had a look in the firmware (F28739D). In that I can't able to find…
Part Number: TIDA-01606 Hi Team,
I am curious looking at this reference design if you have a similar Two-Level Three Phase design similar to TIDA-01606. Do you offer something like this?
Thanks,
Connor
Part Number: TIDA-01606 Dear all,
I'm trying to use TIDA-01606 for the grid-connected inverter but it has too high rated power than I can test.
My test power is less than 1 kW, and the input/output voltages are also changed to 200Vdc/100Vac.
Since I …