Part Number: TIDA-01606 Other Parts Discussed in Thread: SFRA
What is the value of Kpwm in this transfer function. I am not getting that. I referred the above document but I couldn't find it. And what is the delay transfer function (Gd) here and what…
Part Number: TIDA-01606 Dear TI members,
I have a question about gate driver board of TIDA-01606.
I made the same gate driver using reference design as TIDA-01606.
And I powered it up.
And the two green light and one red light turned on(D401, D402,…
Part Number: TIDA-01606 I have some question about gate driver connection.
When I checked the schematic and PCB file, it is different.
Which one is correct?
And also, there is LI_and HI_PWM connection in the main board to gate driver. I am not sure what…
Part Number: TIDA-01606 Dear all,
I'd like to ask about current sensor equation.
When I checked the schematics, the current sensor is shown like below.
And this is CCS code.
where variables are define like the below.
#define TINV_CURRENT_OFFSET_PU…
Part Number: TIDA-01606 Hi TI team
I am trying to build a file.
It is not possible.
It looks like the below.
I have imported the file from the below.
If anyone can solve the problem, please let me know.
Part Number: TIDA-01606 Team,
Customer is testing TIDA-01606 PCB rev 6 using the TMDSCNCD28379D and latest Digital Power SDK 5.00.01.00.
I have made some measurements with LAB7 test mode and the results as below,
We have started initially with 60VAC3…
Part Number: TIDA-01606 Dear experts,
After building a project, I got the below error.
The project file is the reference source code provided by TIDA-01606.
Best regards,
Part Number: TIDA-01606 Hi team,
1) With regard to the relay on the power board, in this project a resistor is placed in parallel on all four relays, what is the purpose of this resistor being placed in parallel? When this resistor is connected in parallel…
Part Number: TIDA-01606 I am trying to open the PLECS file that is provided on the web but after downloading, I am not able to open that even in the MATLAB as it is .slx file. Can you please provide me the PLECS file of that if possible.
Part Number: TIDA-01606 Dear All,,
I am working with the TIDA-01606 for my research.
I have two quesitons about this reference design.
1) Fuse and relay.
When you see the below graph, there is relay and fuse.
But I am not sure how it can prevent from…