Part Number: BQ25798 Other Parts Discussed in Thread: TIDA-050047 , TPS25751 , , TPS25750 , USB-PD-CHG-EVM-01 Hi,
The D+/D- lines are disconnected from the charger in the TIDA-050047.
If I want to use fast charging (for 3S), do the CC lines of the…
Part Number: TIDA-050047 Do you have a 3D CAD file or mechanical specifications for the TIDA-050047? The documents posted on it's web page have 2D information without dimensions.
Thanks.
Hello,
Murugavel R said: Can I transfer .bin file using USBCPD Application Customization Tool to TIDA-050047 using Aardvark Connector?
Yes.
Murugavel R said: if yes will it detect as COM port when I connect into Host machine?
No. It will appear…
Part Number: TIDA-050047 Other Parts Discussed in Thread: BQ77915 Hello Experts,
I am trying to design a balanced charger for a 6000mAh 4S LiPo based on TIDA-050047. For balancing I want to use the BQ77915. Is there a possibility to use only the Balancing…
Part Number: TIDA-050047 Other Parts Discussed in Thread: TPS25751 , BQ25798 , BQ25731 , BQ25713 Tool/software: We are planning to design the Power Bank with below configurations.
Connector type (Input side)
USB Type-C port
…
Part Number: TIDA-050047 Other Parts Discussed in Thread: TPS25751 , BQ25798 , BQ25792 Tool/software: Hi,
I have designed my own power bank solution based on this TIDA-050047 reference design but I can't make it to start charging. Here is the schematic…
Part Number: TIDA-050047 Other Parts Discussed in Thread: TPS25751 Tool/software: I am making a design similar to TIDA-050047, but with TPS25751.
I would like to use the usb for data as well, but I just need USB2 for a microcontroller.
I am a bit…
Part Number: TIDA-050047 Other Parts Discussed in Thread: USB2ANY , BQ25792 Tool/software: Hi,
I purchased TIDA-050047 EVM Board and "UAB2Any" module from Ti Site. After completing configuration, Hardware connect operation seems normal, but during the…
Part Number: TIDA-050047 Other Parts Discussed in Thread: BQ25798 , USB-PD-CHG-EVM-01 , TPS25751 , TPS25750
Tool/software:
Hi
Does TI have a PD Controller+Charger integrated IC? Similar to Infineon: CYPM1115/1116 I can't find the integrated type…
Hi Christopher, Thank you for the reply. So if I understand this well, I can use a design similar to TIDA 050047 but with TPS25751 and I need to have external microcontroller to control both the TSP25751 and BQ25798. Does TI offer different charger that…