Part Number: TIDA-050063 Other Parts Discussed in Thread: TPSI3052 , LM25180
Hi Team,
I'd like to ask you about the value for the smallest size inductor. The customer complained that the size of 560uH inductor(L1) is so big that they can't use it on…
Part Number: TIDA-050063
I am expecting from TI to get response for some of our queries which are mentioned below.
Is TIDA-050063 capable to connect with battery BMS and CAN system?
It would have been helpful for our design if you could share the…
Part Number: TPSI3052-Q1 Other Parts Discussed in Thread: TPSI3052 , , TIDA-050063 Tool/software: Hi,
we are testing on TPSI3052 and identified strange behaviour. When we put 5 V to enable. We measure following at left VDDH and rightVDRV
Also we have…
Part Number: TPSI3052-Q1 Other Parts Discussed in Thread: TIDA-050063 , Hi Expert,
I refer the design guide TIDA-050063 High-Voltage Solid-State Relay Active Precharge
Below is my design Sch,
Currently, I set the Ipeak to 3A, Imin to 0.5A, and adjust…
Dear Bryan,
Thanks for your reply! I probably overlooked these charts in the datasheet, sorry about it.
It is now clear that we can have about 10-12mA on the output of the VDDM.
Two things I would like to further share with you and ask you opinion about…