Hello Ben,
Thanks for posting to the sensing forum!
1) The calculation looks good Ben, my only concern would be with the last line " Checksum = ~Checksum; "
Some compilers might treat it differently and since Checksum is a 16 bit value when in…
Hi Paul,
1. Yes, both interface options drawn are correctly, and will support a SPI/USART bus. There is also the option to use a UART bus, which removes the SCLK pin.
2. This question is not clear.
3. To make a connector change and add a mounting hole…
Thanks for your reply.
But I also have two questions:
1.In TIDA-060024,the way of ground connection is difference between block diagram and schematic,why,which way is better?
2.TIDA-060024 is Mono-static mode,when we use Bi-static mode,is there any…
Hi Rachel,
LDC is great for measuring distances up to 10cm but i am unsure if it will be able to meet your target accuracy. Let me look into this a bit and get back to you. For now i found the following resources available on our website:
What is the…
Hi Gustaf,
The PGA450Q1EVMS_UART_Demo.ino preview was initially released to showcase UART master transmit commands only. It is currently missing the complete ability to receive response data from the PGA450. For any user using this code as a starting…
Hi John,
Is the power question in regard to the PGA460 or the TDA4V?
The TIDA-01597 uses the PGA460-Q1 Ultrasonic Sensor Driver and Signal Conditioner, typically used for automotive park assist applications. A single PGA460-Q1 device operates at a voltage…
Part Number: PGA460PSM-EVM Other Parts Discussed in Thread: MSP-EXP430F5529LP , , ENERGIA , PGA460 , PGA460-Q1 , TIDA-060024
Hey there,
I'm using MSP-EXP430F5529LP and PGA460PSM-EVM. I did connection (the PGA460PSM-EVM 's UART pins to the MSP-EXP430…
Part Number: PGA460PSM-EVM Other Parts Discussed in Thread: ENERGIA , PGA460 , MSP-EXP430F5529LP Tool/software: TI C/C++ Compiler Hi,
I would like to use the PGA460PSM-EVM module to get the distance to the microcontroller (BeagleBoneBlack). I have some…