Hello User,
Welcome to the E2E forum and thank you for your interest in DLP® technology.
The SW21 (green button) is a SW_SYS_ON-OFF switch connected to MSP. Please refer to reference design TIDA-080005 . Unfortunately, there is no option in the firmware…
Hello Jamie,
Welcome to the E2E forum and thank you for your interest in DLP® technology!
DLPDLCR4710EVM-G2 is a display chipset while DLP4710EVM-LC is a light control chipset. Please refer to the [FAQ] Choosing Light Control vs. Display to give you…
Hi Marvin,
For the DLP4710LC, the customer would need to consider two things for their application:
Highest speed streamed random patterns would be 180Hz (three bits per frame, 60Hz VSYNC). The customer would need to know if this sufficient for their…
Hello Tess,
Welcome!
The TI Design TIDA-08005 -"Full High resolution DLP sub-system reference design for high speed desktop 3D printing" is based on DLPC4710EVM-LC.
https://www.ti.com/tool/TIDA-080005
The reference design has all detailed information…
Hello Shayam,
Welcome to DLP forum and thank you for your interest in DLP technology.
The following reference design is based on DLP4710-LC EVM. It includes schematic, Gerber file and BOM.
https://www.ti.com/tool/TIDA-080005
The optical engine used in…
Nobu-san,
The customer will have to uninstall U32 (and all the components associated with it) and connect the Vin net directly to the P12V net in order to change the input supply from 19V to 12V. Please refer to the reference schematic ( https://www.ti…
Vadim,
The stock design of the DLP4710-LC only features the one configuration. However, there are optical engines with the specs that you are looking for available for this chipset.
I recommend you start off by browsing the Optical Module Search Tool…
Hello:
Because no LED is needed in the application, the LED is terminated to form a circuit, but the DMD does not display the example picture, there is no reaction, the power supply and ls_clk are normal,
www.ti.com.cn/.../TIDA-080005
Hi Ivica,
Can you please share the source of information for "Is it recommended to use both input ports, A and B, on the DLP4710 , or one may be left unused". So that I can explain better.
For now, DLP4710 is DMD which is connected to DLPC3479…