Hi Zack,
Our customer has follow up inquiries below.
Thank you for your responses, so I have the last inquiry 1. From the schematic you send me "the frequency band(s) proposed here, the reference design CC1120 Skyworks EM 30 dBm 169 MHz (SWRR111)"…
Part Number: CC1120 Other Parts Discussed in Thread: CC1310 , Hi,
Could someone please guide me with the CC1120 settings to be compatible with the CC1310 standard LRM?
We have tried to settings some settings using the DSSS PN mode. Only receiving CRC errors…
Part Number: TIDC-SIGFOX-CC1120-CC1190-BP I'm working with this kit . As far as I understand, it's just using LNA_EN, PA_EN, MOSI, MISO, GPIO{0,1,2} and CS_N which are pins: P1.6, P3.2, P2.7, P3.0, 3.1, P2.6, P2.3, P8.1, P7.4 and P2.0
This from…
Other Parts Discussed in Thread: CC1125 Hi:
I design a board with CC1125EM 420/470MHz Reference Design(http://www.ti.com/tool/cc1125em-420-470-rd). But unfortunately, I failed.
The observations with my testing are shown as below:
1.It works with SmartRF…
Part Number: CC1120 Other Parts Discussed in Thread: , CC1175 Hi experts,
My customer is using a CC1120EMK-420-470 daughterboard to check operation, but it is not outputting at the value they think they have set for the 429MHz frequency. The host microcontroller…
Part Number: CC1120EMK-420-470 Other Parts Discussed in Thread: SMARTRFTRXEBK , CC1120 Hi,
I'm looking for hardware design files like schematic, gerber files, PCB layout for the CC1120EMK-420-470 .
And I'm also looking for the schematic of the SMARTRFTRXEBK…
Other Parts Discussed in Thread: CC1120 Hi,
I can not find the CC1120 420/470MHz reference design data.
Please put the reference design data to web page.
or would someone please tell me RLC parameter for RF port of CC1120.
The frequency I will use…
Other Parts Discussed in Thread: CC1310 , CC113L Hi!. I`m Eugenio Mercol from Argentina. I`m developer and I need support about "what family of micrprocessor based on RF" could I use for my application?
Project specifications
It should be a microprocessor…
Part Number: CC1310 Other Parts Discussed in Thread: CC1101 , , CC1100E , CC1200 , CC1120
Hi Team,
Now we are using CC1310 on wireless band 470MHz. We want to find a single RF transceiver compatible with CC1310. CC1101 is compatible with CC1310 according…
Part Number: CC1312R Other Parts Discussed in Thread: CC1120
Hi,
My customer want to know if CC1312R have the info like CC1120:
(The following is from CC1120)
– Adjacent Channel Selectivity:
64 dB at 12.5-kHz Offset
– Blocking Performance: 91…