Yes, you can evaluate this using SmartRF Studio 7 : https://www.ti.com/tool/SMARTRFTM-STUDIO
It has a range of output power settings, from +13 dBm to -11 dBm.
Regards,
Zack
Part Number: CC1120 Hi,
we need to design a new system which contains both 434Mhz narrow band (CC1120) and a mesh network based on 868MHz, 27dB PA (CC110x + FEM)
They work on their own antennas (wire or PCB), but async. to each other . The 434Mhz doesn…
Part Number: CC1120 Tool/software: Hi.
We have a scenario where battery life is critical. We are implementing sniff mode/eWor/sleep, minimising the TX power where possible, and minimising packet sizes. We can use : 2-FSK (2 kbps, 2 ksps) or 4-GFSK (4 kbps…
Part Number: BQ24296M Tool/software: Hello.
Our products using BQ24296M have an issue with RF noise that significantly affects on our RF subsystem at 868/915MHz. RF noise from BQ24296M starts when switching converter goes to continuous current mode. …
Part Number: CC1101 Team,
1) Looking at the CC1101EMK868-915 kit ( https://www.mouser.fr/new/texas-instruments/ti-cc1101emk868-915-development-kit/ ):
Q:What module is provided in this kit? Is it: http://www.ti.com/tool/CC1101CC1190EMK915 or http://www.ti…
3) For this you can refer to:
Section 2.2 of SWRA479 ( Achieving Optimum Radio Range ): https://www.ti.com/lit/swra479
Section 2.2.1 of SWRA496 ( CC-Antenna-DK2 and Antenna Measurements Summary ): https://www.ti.com/lit/swra496
Section 4.1 of SWRA328 ( DN031 - CC…
Part Number: CC1120 Tool/software: Hi.
I have three different types of PCBA's using the CC1120. I can TX and RX data with each board. The board are configured as such:
Boards 1 and 2: CC1120 with on-board Johanson broadband 868/923 MHz chip antenna…
Part Number: CC1120 Other Parts Discussed in Thread: CC1125
HI,
I want to use the CC1120 to scan from 868 to 878.6Mhz (±192KHz bandwidth) and detect when a message is sent. The messages modulation is (D)BPSK, 100Hz wide, data rate is 100 or 600 bits…
Part Number: CC1120EM-868-915-RD Other Parts Discussed in Thread: CC1120 Does cc1120 support interleaving and spread spectrum?If CC1120 confirms that these functions are supported, which registers are involved in configuring these functions?
Hello Nir,
I am closing this thread since this is very old and I assume that this issue has been resolved.
Please create new thread if you are still having trouble.
Regards,