Other Parts Discussed in Thread: CCSTUDIO Hello,
For my application OSCCLK is 37.5 MHZ and PLLCR value is 8 to achieve 150MHZ system clock.For flashing this application i guess i cannot use default flash API interface file which is present in CCStudio_v3…
How to compile and upload blinking LED to Olimex TMS320-P28016 using Olimex TMS320-XDS100-V3 emulator under Code Composer Studio 6.1.2?
A couple of important hardware configurations before attempting the connection:
a) The three jumpers of TMS320…
V/Hz -> http://www.ti.com/tool/sprc110 . It is a solution for 24x family, but you should get the gist of it. aci1_10.pdf If you are looking for already made solution Optidrive E3 for Single Phase Motors is one example www.invertekdrives.com/.../ But other…
Hello Maria,
Could you tell me if you see a linker command file in your project folder tree? Files with .cmd extensions are linker command files and are needed in order for the linker to place your compiled code into specific memory regions. Could…
Part Number: TIDC-BLE-TO-WIFI-IOT-GATEWAY Other Parts Discussed in Thread: CC2650 , CC2640R2F , CC3200 Hi,
I want to use the CC2640R2F MCU in place of the CC2650 MCU for the BLE to WiFi Gateway. For this, I need to change the Host Test Project (BLE5Stack…
D:\tidcs\DMC\c28\v32x\lib\doc\data_log.pdf
This module stores the real-time values of four user selectable software Q15 variables in the data RAM provided on the 28xx DSP. Four variables are selected by configuring four module inputs, iptr1, iptr2…
Other Parts Discussed in Thread: TMS320F28044 , CCSTUDIO hi ,
actually I dont know where to post my query.
Iam using tms320f28044,and debugging it in code composer v3.3.during debugging one of the examples I had a problem with this GPIO exmple.…
Hi,
I have seen your posting right now. I'll prepare some document for you to help you. Before this let me answer some questions of you.
I have made some modifications on TI's Ecan-CANB sample programme. I advice you try to make it run first "ecan_back2back…
Dear Friend, Mr. Hareesh,
I tried to run the code send by you. There are two problems.
1. When building the project, the compiler cannot find the header files. I have installed header files from the SPRC191 file downloaded from internet. The installer…