Part Number: OMAP-L137 Other Parts Discussed in Thread: TIDEP-0099 , Tool/software: TI-RTOS I would like to use TIDEP-0099 reference design as a starting point for my project. I have installed CCS and OMAPL137_dsp_setupwin32_1_00_00_11 .
I have a hard time…
Part Number: PROCESSOR-SDK-C6747 Other Parts Discussed in Thread: OMAP-L137 I would like to use TIDEP-0099 reference design as a starting point for my project. I have installed CCS and OMAPL137_dsp_setupwin32_1_00_00_11 .
I have a hard time locating demo…
Part Number: TMDSOSKL137 Other Parts Discussed in Thread: TIDEP-0099 , , TMS320C6747 , OMAP-L137 , OMAPL138 , 66AK2G12 , CC3200 Hi team,
Our I&D project requires audio input, DSP processing and LAN interface as is shown in the attachment. Please can you answer…
Roger,
We are currently only supporting SYSBIOS based Processor SDK RTOS software for new development. The DSP BIOS and pspdrivers are no longer under active development and support.
For MCASP setup with mutli-microphone setup, we do have some demos that…
Hi Carlo,
The LCDK board has been designed to get only Line in input and provide Line out using a stereo AIC31x codec. Stereo codec only allow only two channel (left and right) to be input to DSP using the MCASP codec. You may not be able to exercise the…
Hardik,
Can you please clarify if you are looking for a DSP or an audio converter. Generally voice and audio design would need both to be used for example you can refer to the following TI DEsign on voice that uses AIC3106 and PCM1864 codec with a DSP…
Jared,
I believe these might be interesting to you:
C55x:
Demonstrating Voice Preprocessing on the C5517 EVM
Demonstrating Voice Triggering and Processing with Cloud Connection to IBM Watson
TI design: http://www.ti.com/tool/TIDEP-0083
OMAPL13x…
Hi Steven,
just to confirm we are on same page here is one of configurations (with 8 mic) that I meant
www.ti.com/.../TIDEP-0099
Did you use exactly that one?
BR,
Michail
Jorge,
Just a little bit more information to your questions:
- Differences among C674x DSP and AM570x:
IN addition to performance differences, you will find the C674x DSPs are lower power consumption than AM570x. A good estimate for C674x is …
Part Number: PCM3168A Other Parts Discussed in Thread: TIDA-01454 , TIDEP-0099 , PCM1864 , PCM3168 It's May 2018. Is an EVM for PCM3168A available yet?
If not, when do you think it may be available?
Thanks