Part Number: TIDEP-01017
Tool/software:
Hi,
I'm trying to create a new Cascade Radar Usecases in the PROCESSOR-SDK-RADAR v3.8 using TIDEP-01017.
It is a use case where the radar transmits a signal using my chirp profile and transfers the received…
Part Number: TIDEP-01017 Hello, the angular resolution was shown in Table 3 of the following material.
tidueq8.pdf
Azimuth Array and Elevation Array in Table 3 of this document.
Azimuth Array is written as 86 Element Virtual Array, but it is not…
Part Number: TIDEP-01017 Dear TIDEP-01017 Team,
I would like to develop a real-time demo on the TIDEP-01012. Cesar from this thread
Is it possible to "install" the TIDEP-01017 Software on the TIDEP-01012? Recording to Cesar it is the same HW but…
Part Number: TIDEP-01017 Hi there,
I'm trying to compile the sbl of the processor sdk vision 3.8 usecase tda2xx_cascade_linux_radar under Ubuntu 18.04 LTS. I installed the
gcc-arm-8.3-2019.03-x86_64-arm-linux-gnueabihf compiler under [...]/os_tools…
Part Number: TIDEP-01017 Hi Team,
My customer would like to know which JTAG probe is applicable for TIDEP-01017 via CCS.
Is it possible to use XDS560 v2 STM?
Regards,
Takashi Onawa
Part Number: TIDEP-01017 Hi Team,
My customer just developing their own software using PROCESSOR_SDK_RADER for TIDEP-01017
When they run "gmake -s sbl" in PROCESSOR_SDK_RADER_03_08_00_00 environment, they get MLO files in 4 folders: opp_high, opp_low…
Part Number: TIDEP-01017 Hello!
I use MMWCAS-DSP-EVM + MMWCAS-RF-EVM in cascade radar mimo application with network connection to another board. In cascade_radar_object_detect uscase cfg.mk file configurated to use IPU(01 and 11), dsp1, eve1-eve4. MPU…
Part Number: TIDEP-01017 I try to understand how to work network_tx under Processor SDK radar environment. Is my comprehension OK? I guess two ways of the start to send packets of network_tx.
Unawareness way. C:\PROCESSOR_SDK_RADAR_03_08_00_00\vision_sdk…