Part Number: DP83TD510E Other Parts Discussed in Thread: TLK110 , , TIDEP0032 Question regarding the recent preview of the Ethernet-APL / SPE (10Base-T1L) PHY. I'm curious if this phy could be used for Multi-Protocol Industrial Communications, as exemplified…
Hi HaTa.
Yes it's possible to dynamically switch between Ethernet and Industrial communication based on EtherType as described in the TI design - http://www.ti.com/tool/TIDEP0032
Regards,
Garrett
Part Number: AM3359 Other Parts Discussed in Thread: TIDEP0032
Tool/software: TI-RTOS
Hello, are there any plans to adapt the Multi-Protocol Industrial Ethernet Detection demo (TIDEP0032) to the newer SDK?
And, you tell me what Flash size is needed for…
Hi Sung-IL,
Yes, the multi-protocol can be supported in AMIC110. Please refer to the TI-design "Multi-Protocol Industrial Ethernet Detection With
PRU-ICSS for Industrial Automation' - www.ti.com/.../TIDEP0032 , which describes the mechanism…
Hi Michael, I think this TI design ( www.ti.com/.../TIDEP0032) could be helpful for your use case
TI design document: www.ti.com/.../tidua28a.pdf
thank you,
Paula
Hiroyasu, For your reference, we have a "Multi-Protocol Industrial Ethernet Detection w/PRU-ICSS for Industrial Automation" TI design.
www.ti.com/.../TIDEP0032
www.ti.com.cn/.../tidua28a.pdf
thank you,
Paula
Hi Arron, The PRU compiler inside CCS is installed via the CCS App Center (View-->CCS App Center), or alternatively here: software-dl.ti.com/.../download.htm There are (some) syntax changes in the source code required to port the assembly code from…
Isolation University.xlsx
Matthew,
I have attempted to include an excel sheet from the Isolation Department's ISO University. It contains several links to collateral explaining isolation and it's applications. If the attachment failed, type "iso/" in…
One more question, Our requirement is to use multiple industrial protocol simultaneously. (Profibus, Profinet, BACNet, ModBus and Ethernet IP) Below diagram stats that we can not. www.ti.com/.../schematic_tidep0032_20160309101111.jpg Can you please…