Part Number: TIDM-02011 Other Parts Discussed in Thread: C2000WARE Hi expert,
I am supporting customer on test LFU demo.
and I have some questions:
1. I can see a bankSelect function, which will goto the newest bank. but I can not find where we update…
Rana,
Please refer to section 4 of tiduey4. This is the design guide of TIDM-02011, and section 4 is a FOTA section.
We do not currently provide a CAN Flash kernel example for F2837x, but you can use the example from F28003x for DCAN (in C2000Ware at driverlib…
Hi Manish,
We have the Live Firmware Update (LFU) TIDM-02011 reference design that should be able to provide you with the example code.
For more information, please take a look at these application notes:
https://www.ti.com/lit/pdf/spruiu8 (LFU w/ a device…
Part Number: TMS320F280039C Other Parts Discussed in Thread: C2000WARE , TIDM-02011 Does TMS320F280039C also have the example code like T MS320F28004x,
flashapi_ex3_live_firmware_update
flashapi_ex5_lfu_no_reset
I did not find the above exmaple for TMS320F28003x…
Hang,
Yes, alternate versions will use alternate linker cmd files, this is understood. But there is no additional relationship between the "exact version name" and the linker cmd file. As long as the alternate versioning relationship is maintained with…
Part Number: TMS320F280049C Other Parts Discussed in Thread: LAUNCHXL-F280049C , C2000WARE , TIDM-02011 Tool/software: Hi,
I wanted to perform Live firmware upgrade and referring SPRUIU8a, following the steps as mentioned in 6.2.
Hardware Used: LAUNCHXL…
Part Number: TMS320F28388D Other Parts Discussed in Thread: TIDM-02011 I have Controller (TMS320F28388D). I Plan to live firmware update without device reset on F2838x( TMS320F28388D ) MCUs via SPI. For this, please provide a reference document or application…
Zhentao,
The 1st option (A/B swap) is not supported on F28x devices.
The 2nd option is supported. Please refer to our LFU reference design TIDM-02011 available within the C2000 DigitalPower SDK.
Thanks,
Sira
Part Number: TMS320F280049 Other Parts Discussed in Thread: TIDM-02011 Hi all,
My customer needs urgent support on this issue. They found that the global/static variables are not initialized after LFU.
They called _c_int00 after LFU, but the variables…
Part Number: TMS320F28386S Other Parts Discussed in Thread: C2000WARE , TIDM-02011 Hi,
I am trying to develop a project which will have:
1. A customer/secondary flash bootloader which is located in flash sectors 0 & 1, on the core CPU1.
2. An application…