Part Number: TIDM-02013 Hi,
We are going to launch a order of 10 units of TIDM-02013 and once we receive the boards we would like to safely test them. Is there any way to test the AC/DC (PFC part) and DC/DC (CLLLC part) independently?
For example, for…
Part Number: TIDM-02013 Hi,
The TIDM-02013 ref design is for Single-phase 7.4KW.
I want to design a 3 kW OBC.
my output requirement is 60 VDC @ 50 Amps
ALSO please let me know how
1. I can run the code is written for TIDM02013 on my custom Power Board,…
Part Number: TIDM-02013 Hi,
With this reference design, would it be suitable to use TMS320F28075 from C2000 series. This MCU has higher pin count.
But we want to check if functionally it is suitable to run the digital control algorithm required for the…
Part Number: TIDM-02013
Can the charger output voltage be changed to 84V through firmware?
I've ordered the product but was unsure regarding if the charging profile was according to my application.
The Docs say that the output would be 350V.
The input…
Part Number: TIDM-02013 Hi Champ,
I am asking for my customer about the SR control implementation in TIDM-02013.
(1). Is the the control mechanism of SR is to compare ISEC_TANK nearly to 0A, then shutdown the SR ?
(2). Can SR enable and have the duty in…
Part Number: TIDM-02013 The PAMC3302DWER IC is used for current measuring on the PMP22773 board which is part of the TIDM-02013 reference design. However, this IC is now discontinued by the manufacturer so is there a replacement IC that could be used ideally…
Part Number: TIDM-02013 Hello experts,
Why most of the single phase pFC output is kept at 400V ?
is it because of any kind standards limiting Single phase PFC out at 400V ?
Incase of any kind of requirement demands more output voltage, it can be achieved…
Part Number: TIDM-02013 Other Parts Discussed in Thread: C2000WARE Sir,
Our startup is developing a Solar MPPT based hybrid power supply of ratings 5kW and input solar voltage will be 190V - 450V DC and MPPT output will be 400V DC. This 400V DC will feeds…