Hi,
There are many relevant reference designs in the block diagram.
Is there one design for solar power optimizer?
TI provide may digital power application design.
For examples,
TIDM - 1000 : vienna rectifier
TIDA - 01606 : T Type bi-directional…
Thank you for your prompt reply.
We are having occasional freezes of the ccs or crashes where it stops responding, though the 1142 errors happen more often in the following ways.
Sometimes I get just that 1142 error when I run the debug or run, though…
My apologies for the typo in my response. For fastest calculation of trigonometric function please use TMU instructions available in many of our latest MCUs.
TMS320F28069 does not use these TMU instructions. However you can use the CPU power to calculate…
Hi Francois,
TIDM-1000 supports both Piccolo TMDSCNCD280049C Control Card and Delfno 2837x control Card as you can see in the digital power sdk. Thanks.
Regards,
Chen
Abdin,
Its best to create a new projectspec in the C2000ware-digitalpower-sdk solutions folder under devices / new devices/ ccs
following document outlines the steps,
system_solution_porting_guide.pdf
There is no ccs project for a particular control card. The CCS projects are based on application. You should be able to use CCS Help menu to see some of those you mentioned.
Download latest C2000Ware and you will see several applications. For examples…
Hi Nicola,
We would also like to point to the following two designs as they will both be able to handle 3 phase AC/DC conversion uni-directional for the first one and bi-directional for the second one.
TIDM-1000 (2.4kW) (700VDC)
Vienna Rectifier…
What types of topologies are available for the digital power SDK? Does the SDK generate code for controlling phase shifted full bridges and similar?
In general does this SOC support multiple control loops operating in parallel?
DP SDK has quite…
I have used 10k as pull downs in many schematics. see TIDM-1000.
But please note, many Automotive grade gate drivers will have an enable disable pin, and this pull down is an optional protection if one uses the gate driver enable disable.
I have added…