Part Number: TMS320F280049C Other Parts Discussed in Thread: TIDM-1000 , SFRA Hi Team, Greetings of the day!. We are designing custom PFC board and referring the Design Guide TIDM-1000 of Vienna Rectifier. We have a doubt on the TIDM-1000 compensation…
Part Number: TIDM-1000 Other Parts Discussed in Thread: TMDSCNCD28379D ,
Tool/software:
Hi,
I am working with TIDM-1000 board using the control board TMDSCNCD28379D, when I am starting with BUILD1 configuration, getting the output as shown below…
Part Number: TIDM-1000 Other Parts Discussed in Thread: C2000WARE Tool/software: Hi Team,
I am currently testing different builds for TIDM-1000 (Vienna Rectifier) with F28004x control card. The firmware version is C2000Ware_DigitalPower_SDK_5_02_00_00…
Part Number: TIDM-1000 Can I put LLC converter in each half bus of the vienna recitifer whether it cause any issue. Or i should put the LLC DC to DC converter only on full bus output of the vienna rectifier.
Part Number: TIDM-1000 Other Parts Discussed in Thread: TIDM-02013 Hi,
I don't quite understand this part of the inductor voltage drop feedforward,the screenshot of the program is as follows
I looked at other thread but didn't get an answer that…
Part Number: TIDM-1000 Hello
I want the operate the tidm 1000 with input frequency 400 Hz
So I have modify the code , VIENNA_MAX_GRID_FREQUENCY = 500 Hz previously it is 110 only
Case 1 : I have checked the output with Input voltage 115 V, 250 HZ…
Part Number: TIDM-1000 Other Parts Discussed in Thread: PMP23069 I want to operate 3-Ph Vienna rectifier even after when an abnormal state of single phase failure and two phase failure occurs and after some time it comes back to normal steady state. …
Part Number: TIDM-1000 Other Parts Discussed in Thread: SFRA Hi Team,
Greetings of the day!
We are using TIDM-1000 Software for our custom board with our ADC scale factor and Passive element parameters.
Now we want to change compensation designer…
Part Number: TIDM-1000 Hello
As per TIDM-1000 reference design document, can you please explain the DC bus capacitor formula is derived. The same formula can be used for 2 level and 3 level Active front end converter while connecting inverter as load…
Part Number: TIDM-1000 Hi Team,
Here're some issues from the customer may need your help:
1. In the VIENN rectifier, is the inductor behind the current transformer used for filtering?
2. The maximum input current written in the manual is 4A, so…