Part Number: TIDM-1007 Hello,
We are referring TIDM-1007 for AC-DC PFC design. We wanted to do some modifications in the design using your power design tool i.e. Webench
In AC-DC designer using these parameters:
Vin_Min = 90 VAC
Vin_Max = 270VAC…
Part Number: TIDM-1007 Other Parts Discussed in Thread: TMS320F280049 , C2000WARE , TIDM-02008 Dear team:
TIDM-1007 & TMS320F280049
C:\ti\c2000\C2000Ware_DigitalPower_SDK_3_01_00_00\solutions\tidm_1007
My customer wants to know the corresponding…
Part Number: TIDM-1007 Hi all:
An error occurred when one of my clients opened the TIDM-1007.PrjPcb (schematic & PCB) hardware data in TIDM-1007.
The following information is displayed:
STG: docfile has been damaged
He has changed 3 PCs with…
Part Number: TIDM-1007 Other Parts Discussed in Thread: TIDM-02008 Hello team,
My customer is evaluating TIDM-1007 for their design and wanted to know if it is possible to enable/disable the inverter output by either hardware or software. They would…
Part Number: TIDM-1007
Hello TI Experts
I"m Currently working with Totempole PFC Converter and following your interleaved Totempole PFC Design. In the schematic file you have provided, the input side AC voltage, ACL_SENSE and ACN_SENSE points are…
Part Number: TIDM-1007 Other Parts Discussed in Thread: TIDM-02002 , TIDA-010054 Hi,
1. AC-DC stage of 3.3KW we can use TIDM-1007
2. For DC-DC stage after that we need 60-85Vdc output. Is there any reference board available which we can use?
Part Number: TIDM-1007 Hi experts
we're evaluate a CCM totem pole solution . Referenced from TIDM-2008/TIDM-1007 . The AN shows the control timing of active mos and sync mos ,the sync mos is turned on after active mos finished duty-softstart.
I also…
Part Number: TIDM-1007 Other Parts Discussed in Thread: POWERSUITE , , TIDM-02008 , SFRA Dear all,
in the process of trying to implement 3 current loops instead of just one, I've performed measurements on CPU usage, just to make sure there is enough…
Part Number: TIDM-1007 Other Parts Discussed in Thread: POWERSUITE , Dear all,
in the process of trying to implement 3 current loops instead of just one, I've performed measurements on CPU usage, just to make sure there is enough time to do it with…