Hi Rhea,
Sorry, I misunderstood your question in my initial reply and didn't look at the AD2S1205 device datasheet. You are wanting to interface with the digital side of the AD2S1205 device then?
The datasheet provides some reference below where a…
Part Number: TMS320F28377S Other Parts Discussed in Thread: TIDM-1010 , TMS320F28379D Hi~
I have a question about the 28377S and BISS-C communication connection.
Referring to the document below, it is explained that BISS-C communication is connected…
Part Number: TMS320F28379D Other Parts Discussed in Thread: TIDM-1010 Hi,
About "TIDM-1010 : BiSS-C Absolute Encoder Master Interface Reference Design for C2000 MCUs reference design", TMS320F28379D is used.
My customer would like to know if the FW…
Hello Huseyin,
Huseyin Kahraman said: 1- Can I communicate with the encoder whose link I shared using your BOOSTXL-POSMGR product?
We use the BOOSTXL-POSMGR for connecting to encoders supporting BiSS-C, T-format and EnDat22 encoder protocols. Note…
Part Number: LAUNCHXL-F28379D Other Parts Discussed in Thread: BOOSTXL-POSMGR , , TIDM-1010 , LAUNCHXL-F280049C , CONTROLSUITE
Tool/software: Code Composer Studio
Hi,
I am using the LAUNCHXL-F28379D launchpad. I will use an absolute encoder using…
Hello,
TI has available a TIDesign for the BiSS-C encoder interface. The source code for the library is not available but the documentation it may give you some ideas.
The design uses the CLB to clock the SPI and the encoder clock (MA line) as required…
Dorion Carr said: Then it "appears" that ePWM1 is setup in the CLB global inputs to connect to Tile 4 in CLB_IN0 what is this doing in the CLB code example. Is it helping to provide the BissC and SPI clock?
No, none of the ePWMs are used as an input…
Part Number: TMS320F28379S Other Parts Discussed in Thread: TIDM-1010 , CONTROLSUITE , BOOSTXL-POSMGR Hi,
I was wondering if the BiSS library (as in TIDM-1010) can be used on the 28379S device?
any modifications needed?
We're doing PMSM FOC application…
LEE Jea kyung said: If BISS-C communication is possible, what circuit should be configured for BISS-C communication?
Hello,
Please refer to this TI Design: https://www.ti.com/tool/TIDM-1010
Regards
Lori
Hi. F28335 doesnt support BiSS-C interface. Newer devices, with Configurable Logic Block (CLB) F2837x etc., support BiSS_C interface. Please refer to http://www.ti.com/tool/TIDM-1010 Also, SPI or McBSP interface is not directly compatible with BiSS-C…