Part Number: LP-CC1311P3 Other Parts Discussed in Thread: SYSCONFIG Tool/software: I'm trying to shut down the MCU after 3 blinks each time I wake it up. but the wake-up pin acts as a gate and shutdown immediately, without the blink. Here's the attached…
Part Number: LP8866-Q1 Tool/software: Hello, I need to consult the following questions about LP8866: 1, there are 19 LED, 2 series (10+9), each series needs 500mA current, as shown below the connection mode can work normally? Is there a problem?
2…
Part Number: BQ24171 Hi Jeff:
I have a question about the status of LED lights that I would like to ask you
In the following video, during actual use, after connecting the battery, the LED occasionally appears as shown in the video (flashing first…
Part Number: LP5861 Hi team,
My customer faced a problem during using our LP5861. They found that they cannot control the CS pins.
The schematic is attached, and first you can help review the schematic, whether it has any problems.
LP5861 Schematic…
Part Number: TIDM-1000 Hi experts,
I am testing TIDM 1000, and am confused about some code and control algorithm.
Q1: How can an offset added to duty cycle control the DC voltage balance?
Q2: What is the effect of inductor voltage drop feed forward…
Part Number: DLPLCRC410EVM Other Parts Discussed in Thread: DLP7000 , I am using a DLP7000 connected to a DLPLCRC410EVM and sometimes the D2 LED stays lit red and does not work properly. However, when I turn it on again after some time, it works normally…
Other Parts Discussed in Thread: AFE58JD28EVM Team,
We got 3 TSW1400EVM. 2 of them show D6 D7 LED doesn't light up. D5 lights up and indictates ADC CLK is in. Their FPGA firmware was not touched. We are on Win11 system, providing 5V supply with 5A…
Part Number: TL431 Tool/software:
Hello everyone,
I have designed a circuit which is powered by a 3.7V LIPO battery. This supply voltage passes through a LDO (IC1 in the schematic) which regulates the voltage to 3V to feed a small DC motor (+3V_MOTOR…
Hello Aaron ,
You can't determine the cause of D6 turning red from the log I sent you last time can't you?
Our current situation is that we have connected the PC, EVM, Front-End, and DMD boards together and have confirmed using the GUI that the PC…