Part Number: TMS320F280049C Other Parts Discussed in Thread: TIDM-DC-DC-BUCK Hello,
the TIDM-DC-DC-BUCK example for F280049C works very well when launched from debugger. However, it does not seem to start once the microcontroller is reset.
Judging…
Part Number: LMG5126 Other Parts Discussed in Thread: LM5155 Tool/software: Hello,
My customer is looking for DC/DC boost ICs that can support the following conditions.
CASE1 - Input : Battery 3.7V / 10A, Output : 28V / 7A
CASE2 - Input : Battery…
Part Number: TIDM-02002 Other Parts Discussed in Thread: POWERSUITE , , TIDA-010054 Greetings, I am currently looking for a bidirectional DC/DC stage solution for a system similar to one described in a following block diagram: https://www.ti.com/solution…
Part Number: LM25574 Other Parts Discussed in Thread: LM5137 , LM5149 , LM5148 Tool/software: Hi experts,
As a fresher engineer, designing a power supply board, I need your suggestions on how to approach the design process, where to start, and how to…
Part Number: MCT8316Z Tool/software: I want to use the built-in DC/DC converter and LDO regulator for "bootstrapping" my MCU (a Renesas RA0E1).
However, when applying VM (12V, in my case), the DC/DC won't start up.
Is there any pin (apart from the…
Part Number: TIDM-DC-DC-BUCK Other Parts Discussed in Thread: LAUNCHXL-F28379D Tool/software: Code Composer Studio Hello,
I am trying to modify the PWM frequency of the TIDM-DC-DC-Buck reference design to suit my project specification (Buck converter…
Part Number: LM5157 Tool/software: Hi Team,
My boost converter is intended to operate in a bypass or idle mode under normal conditions and activate only when the input voltage falls below 6.9 V, in order to sustain the output voltage above 6.9 V with…
Part Number: LM5149 Other Parts Discussed in Thread: LM5148 , LM5148-Q1 Tool/software: Hello,
can LM5149 at HO+LO pins drive GaN transistors? Hence, the gate source voltage is maximum +5V?
Sourish,
Debug of system-level issues on customized applications is typically the responsibility of the developer. It is also not practical for us to attempt complex debug remotely.
Would you be able to hone in on a specific malfunction that TI supports…
Part Number: UCC14240-Q1 Tool/software: hello.. i m gona design a isolated RS-485 master full-duplex transceiver to 8 RS485 slave tranceivers (camera) reference from below website, and hence i need a isolated DC/DC buck converter from 12v to 3v3. I m…