Part Number: UCC28220
Hello,
I would like to know if this can be used to implement an interleave DC-DC buck converter, for example. I would like to know the steps from high voltage (800V) to low voltage (100V) without current at 60A.
I am trying…
Part Number: TMS320F28379D Other Parts Discussed in Thread: LM5171EVM-BIDIR , LAUNCHXL-F28379D , LM5171 , C2000WARE Tool/software: Hello,
I want to use LM5171EVM-BIDIR as a bidirectional dc/dc converter to charge a supercapacitor bank and discharge…
Part Number: UCC28750 Tool/software: Hi TI Team,
Good Day!
I would like to know if it’s possible to achieve an isolated DC-DC conversion from 400V to 12V using the UCC28750 without using a transformer.
If yes, could you please share any available…
Part Number: TPS631010 I designed a 3V to 1.8V dc-dc regulator and 3V to 3.3V dc-dc regulator using TPS631010YBGR (buck-boost regulator).
A maximum current of 51.1mA is drawn from 1.8V regulator and 240mA from 3.3V regulator. The 3.3V regulator supplies…
Part Number: LM5146-Q1 Other Parts Discussed in Thread: LM70860 Tool/software: Thank you, Tim. I have checked the quick start calculator and have attached the Excel sheet for your review. Please let me know if any changes are needed. Untitled spreadsheet…
Part Number: LM61495 Tool/software: Hi everyone,
I’m working on a heater application and want to design a DC-DC converter with a 34V input and an adjustable output voltage between 15V and 30V. The heater has a resistance of 6.4 ohms.
Due to limited…
Part Number: LMZ23605 Tool/software: Dear Sir/Madam,
We want to use LMZ23605 DC-DC Converter for new design. Please provide the life time and also mention is it recommended for New deign,Active or not.
And also suggest the Isolated and Non-Isolated…
Part Number: TMS320F2800132 Other Parts Discussed in Thread: PMP
Team,
Do we have some specific collateral for realizing a Bi-directional DC/DC Buck-boost using C2000?
-I have seen the below but this seems out dated: UG for C2000 based TIDM-BUCKBOOST…
Part Number: LMR43620 Hi Dear,
The customer has a demand for a DC DC Buck . The specific requirements are that the input terminal supports 9-36V, the output is around 21V, the current is 2-3 A, and the ripple should be as small as possible, around 10…
Part Number: LM65680-Q1 Other Parts Discussed in Thread: LM65680 , LM76003 Tool/software: Hello everyone and TI teams. I am currently designing my board's power stage which would ideally allow to convert one 36Vdc line in two separate lines:
- A 24Vdc…