Part Number: UCD3138 Other Parts Discussed in Thread: TIDM-1000 ,
Tool/software:
TIDM-1000 reference design | TI.com
In the TIDM-1000 schematic, the inductance value of PFC inductor (53PR116-292) L2/L4/L5 is 2mH, with a peak current of approximately…
Part Number: C2000-F28004X-POWER-EST-CALC Other Parts Discussed in Thread: TIDM-1000 , C2000WARE Tool/software: In the TIDM-1000 schematic, the inductance value of PFC inductor (53PR116-292) L2/L4/L5 is 2mH, with a peak current of approximately 15A. According…
Part Number: TIDM-3PHMTR-TAMP-ESD Other Parts Discussed in Thread: MSP430F6779 , Tool/software: Hi,
We are using TIDM-3PHMTR-TAMP-ESD reference design hardware for smart meter development which uses MSP430f6779 controller.
We are using firmware code…
Hello Support,
Thank you for your assistance. Following your valuable suggestion, we have decided to proceed with the purchase of the MSP430 CaptiVate devices. While reviewing the product specifications, I came across a mention of an EVM kit that accesses…
Hi Hang,
Appreciate you clarifying the requirements. Can you clarify a few more items:
- Do they need DFU without POR?
- Is DFU with a reset acceptable e.g. like a Watchdog reset? If yes, we have an example for that in the TIDM-02011 F28003x Flash…
I assume the order would be
1. Download the software
2. Remove the said jumpers
3. Start the Energy Trace.
Observations
I can not start Energy Trace/Energy Trace++ before starting the debug process, in CCS Theia(with all jumpers connected…
Hi Jeff,
I have connected 10uF cap on BAT and set 0xD5. root@imx8mp-lpddr4-evk:~# dmesg | grep "bq257*" [ 8.917583] bq25790-charger 0-006b: Line 998: Watchdog timer: 2000 [ 8.917605] bq25790-charger 0-006b: Line 1007: Input voltage limit: 4500000 […
Part Number: TIDM-02012 Other Parts Discussed in Thread: SYSCONFIG Dear Forum,
I am trying to get the TIDM-02012 eCompressor example running with a custiom motor.
I have a multitude of problems:
With the example from SD 4.01 I manage to run my hardware…
Target Application: Automotive Energy Management Products
MCALs required : We are using following Peripherals from sysconfig >> DIO, ePWM, ADC, CPU Timer, Watchdog, MemCfg, MCAN, PCAN, DAC, SPI, I2C, ECAP, FSI, CLA.
Part Number: TIDM-02009 Other Parts Discussed in Thread: TIDM-02000 Hi,
I'm investigating the modes of operation of SR at PSFB CDR topology.
I saw that TI implemented different SR modes.
Mode 0 as no SR's are driven. SRs are only driven at diagonal…