Part Number: TIDM-SOLAR-DCDC Hi all I referred the above mentioned project to build a MPPT boost converter. It used analog comparator output to limit the output voltage of the boost converter by feeding it to the pwm output with CBC trip option. Voltage…
Part Number: TIDM-RESLLC-DCDC Other Parts Discussed in Thread: TIDM-02002 , TIDM-1001 We design step-up power module, DC48V input, output 90V, power 2000W, output with constant current and short circuit protection。Select the output up to 60V or 72V by switching…
Part Number: TIDM-PSFB-DCDC
Hi Team,
Our customer tried to open the TIDM-PSFB-DCDC schematic diagram using Altium but it seems the file is empty as shown in the screenshot below. Is the schematic diagram in Eagle format. If not, which design software it…
Part Number: TIDM-SOLAR-DCDC Hi!
Thank you for your answers.
Altium designer could'nt open cad files( .sch & .pcb ) .how should i open these files
(C2000™ Solar DC/DC Converter with Maximum Power Point Tracking (MPPT) )
TIDM-SOLAR-DCDC
…
Part Number: TIDM-SOLAR-DCDC I have an application where i would like to modify the TIDM-SOLAR-DCDC design to as a 2 stage converter as follows
Stage 1 : 2 phase boost : Input 5-30V , output 65V ,500W, regulates input current . Don't need MPPT ,Needs new…
Part Number: TIDM-SOLAR-DCDC I see another post reported problems with the Gerber files.
What exactly are the problems ?
What needs to be fixed ?
I think it would be good if TI can get this a addressed . This is a reference design so this should be fixed…
Part Number: TIDM-SOLAR-DCDC Tool/software: Code Composer Studio Hi!
Thank you for your kind answers.
We will purchase a development kit for TI products to develop a 3kW dc-dc booster converter.
(C2000™ Solar DC/DC Converter with Maximum Power Point Tracking…
Part Number: TIDM-PSFB-DCDC Other Parts Discussed in Thread: C2000WARE Hi team,
My customer wants to evaluate the TIDM-PSFB-DCDC design performance. So how can I apply for a TIDM-PSFB-DCDC demo board or if customer could purchase it on TI store? Thanks…
Part Number: TIDM-HV-1PH-DCAC Other Parts Discussed in Thread: TIDM-SOLAR-ONEPHINV , CONTROLSUITE Dear,
For our development, we can't use a single inductor for switching, so we have to add a second inductor to the low-frequency bridge.
Can you give…