Part Number: TIDM-SOLARUINV Other Parts Discussed in Thread: TIDM-HV-1PH-DCAC the same for the TIDM-HV-1PH-DCAC;
it is not much clear from the EVM page...
thanks a lot in advance
KR
Vincenzo
Part Number: TIDM-SOLARUINV hello ,
can anyone confirm be the below details for TIDM-SOLARUINV.
Following confirmation is required for sample PCB manufaturing.
Inner core is 70 Microns = 2 Oz ? 2) Outter Layer is 105 Microns = 3 Oz ? 3) Non ROHS ? 4)…
Part Number: TIDM-SOLARUINV Tool/software: Code Composer Studio Hi, I am testing the state machine for grid connection with the solar micro inverter and I having some problems with some states. When the micro inverter board is in Idle state and I give…
Hi Shamim,
Thank you for this detailed answer! I would have some more questions though:
Shamim Choudhury said: The first stage boost the voltage to 40VDC
I guess that you meant 400VDC for the DC bus of the TIDM-SOLARUINV kit, right?
If it the case, would…
Hello Vaibhav,
I would like to implement grid syc feature with this design. I can see multiple main.c files. None of them having grid sync or changer over feature implemented.
This code examples was written for testing of TIDA-01292 so we have worked…
Other Parts Discussed in Thread: TIDM-SOLARUINV Hi , TIDM-SOLARUINV reference design is having a capacity of 280W.I want to develop same grid tie inverter with 1KW capacity. Kindly suggest me the is it possible to develop for 1KW?
Regards, Santosh B …
This is the closest design we have
www.ti.com/.../TIDM-SOLARUINV
it is controller using a programmable solution, C2000 MCU for which you can write code to get the desired behaviors.
Part Number: TMS320F28035 Hi team,
A customer needs help in getting started with Solar Micro Inverter Development Kit [ http://www.ti.com/tool/TIDM-SOLARUINV ].
The customer is trying to understand how the inverter GUI works. He was able to run the dispatch…
Jerry,
yes it can be with a F28069 controller,
we also have some reference design for the DC-AC
TIDM-HV-1PH-DCAC which uses F28004x
and also a solar micro inverter
which has a DC-DC and a DC-AC
TIDM-SOLARUINV
however the power and volatge levels…
Ricardo, we have two TI reference designs that relate to Grid Tie Power Inverter application. They are TIDM-SOLARUINV and TIDA-01606. For both, you'll find detailed schematics, Design Guides, and bill-of-materials (BOMs). Hope that this helps. …