Other Parts Discussed in Thread: DRV8301 , DRV8313 Hello,
I recently completed a test that required control of eight BLDC motors (48V/5A/10k RPM) using eight DRV8301-HC-C2-KIT eval boards running lightly modified Instaspin software and a Stellaris Launchpad…
What is the voltage? I'm going to assume if 200W you are probably at 12 or 24V. The HVMTR+PFC is 50-350V bus, 10A. What I would suggest is the DRV8301-HC-C2-KIT. This is up to 60V, 60A and also includes the F28035.
The included projects with this…
Isolation University.xlsx
Matthew,
I have attempted to include an excel sheet from the Isolation Department's ISO University. It contains several links to collateral explaining isolation and it's applications. If the attachment failed, type "iso/" in…
Part Number: DRV8302-HC-C2-KIT Hello,
I am using the DRV8302-HC-C2-KIT for a senior design project. I am using it to control a BLDC motor for a small car. In order to use the motor from the board I am also using an analog foot throttle. I was able to…
Hi Samhitha,
Thanks for your reply.
I share three build logs and try cleaning and building behavior. "alg_lib project build log" is the library project build log we created based on the instructions in the previous article. "project with alg_lib…
Part Number: MSP432P401R Tool/software: TI C/C++ Compiler I have an object file built with TI Arm compiler 16.9.4 LTS. I am using armofd from the same release to extract .debug_info and .debug_abbrev sections. DIE for a variable is missing the attribute…