Bob,
The DK board is brand new and I am the only one using it. Good news is that I am able to recover and set the FLASH_BOOTCFG register to its default value of 0xFFFFFFFE. I read the datasheet, there is no way that I can manually program the register…
Hello Gute,
gute1 said: unfortunately the TM4C123 does not have a high-speed built-in (only with external device)
TM4C123x I don't think can support high speed in any situation.
TM4C129x devices can support USB 2.0 High-speed using an external PHY…
Hi Bala, The KSZ8463FML PHY can have its SPI interface put in MIIM mode which is the Serial Management Interface (SMI) that is the standard interface to program the PHY. Did you put the KSZ8463FML PHY in MIIM mode and use the MCU's MDIO and MDC signals…