Part Number: TIOL111 Hello
My customer has an question for NFAULT behavior during wake-up pulse in TIOL111. TIOL111 on their board detects wake-up pulse correctly, but NFAULT signal also goes to low at the same timing as the wake-up pulse like the below…
Part Number: TIOL111 Hello guys,
One of my customers is considering using TIOL111 for their next products work with their original interface similar with IO-Link.
But the power line voltage (L+) is 48V. So could I ask you the following question?
Q.Can…
Part Number: TIOL111 Hello,
TIOL111 datasheet defines I_REV (Leakage current in reverse polarity) as the below figure. Do you have temperature drift data for this I_REV with "EN=HIGH, TX=LOW; V(CQ to L+) = 3V" condition (marked with yellow)? …
Part Number: TIOL111 Hi All,
We are studying a possible solution with TIOL111x IO-Link transceivers with integrated surge protection.
In the datasheet (page 5) the quiescent current is given in the case of enable low and high without load. It is not said…
Part Number: TIOL111 Hello,
customer ask what pull up resistor sizes for the WAKE and NFAULT pins are valid. He uses a MCU with internal pull ups of min 20Kohm and max 60Kohm.
Regards, Holger
Part Number: TIOL111 I use TIOL111 to implement the IO-LinK Communication.
when the master node change the CQ Level or transmit data on CQ Line, Whether the Wake signal transmitted to the device node automatically ?
Do I need configure some register for…
Part Number: TIOL111 I want to use TIOL111 in my design. i want to derive L+ and L- internally of my PCB and only i want to expext CQ externally. Can i do like this or not ?