Part Number: TIR1000 Other Parts Discussed in Thread: STRIKE Dear Specialists,
My customer’d like to confirm maximum input voltage rating.
I would be grateful if you could advise.
---Question
According to the datasheet, the maximum rating of input…
Part Number: TIR1000 Dear Specialists,
My customer is considering TIR1000 and has a question.
I would be grateful if you could advise.
---
About 6 pins (IR_RXD) of TIR1000,
The pulse width of the input signal is described as 3/16 clock at datasheet P…
Part Number: TIR1000 Hello experts,
Does TIR1000 have external clock timing requirement like MCP2122 (datasheet P22)?
MCP2122 https://www.microchip.com/wwwproducts/en/MCP2122#datasheet-toggle
I would appreciate if you would give me comment about external…
Part Number: TIR1000 Other Parts Discussed in Thread: TL16C550C Hi,
In a design we are planning to implement IR Data transmission (Transceiver) at lower speed maximum of 115200 bits/second. I found this part TIR100 can do the Job but I have few doubts…
Part Number: TIR1000 Other Parts Discussed in Thread: BOOST-IR Hi,
For a lift project we have to communicate data via optical interface and we would have identified the TIR1000PWR as IrDa Encoder / decoder.
We should not follow a particular standard but…
Part Number: TIR1000 Other Parts Discussed in Thread: SN74LVC1G125 Hi,
I am developing a PCBA which uses this part. It connects between a TFB4711 and a ATSAMA5D27C CPU. All the UART ports are used up on the CPU, so I want to share the TIR1000 with the…
Part Number: TIR1000 Hello team,
We can see a description on "When a falling edge is detected on IR_RXD, U_RXD falls on the next rising edge of 16XCLK with sufficient setup time ." in the section "7.4.2 IrDA Decoder Function". How long…
Part Number: TIR1000 Dear all.
I'm looking for an IR remote control decoder that supports NEC format. Based on the TIR1000's search for IrDA Encoder & Decoder, NEC Format does not appear to be supported, is it possible? I'd like to ask you…
Part Number: TIR1000 Other Parts Discussed in Thread: MAX232 , TL16C550D Hi, Im using a TIR1000I for interfacing a PC UART ( setting a MAX232 before TIR) and in the other side the microcontroller, but I need to change baudrate often. In the side of PC UART…
Part Number: TIR1000 Hi,
My customer need a IrDA to Uart function. looks like TIR1000 is suitable and without the SW need. Here, want to know Can TIR1000 directly connect to MCU like msp430? any reference circuit and sample code?