Part Number: MSP430FR6972 Other Parts Discussed in Thread: TIR1000
Tool/software: Code Composer Studio
Hello,
I am using MSP430FR6972 with TIR1000.
My plan is to receive data through IRDA(Rx pin of UART1) and send that data to Serial Monitor via 'UART0…
Part Number: TIR1000 Other Parts Discussed in Thread: TL16C550C , SN54LS674
Hello,
I ordered a few mpc2221 chips from Microchip. It is a small chip that is capable of converting usb signal to vitual RS232 signals. I also ordered some leds from Vishay…
Part Number: TIR1000 Dear Team,
Could you please help to review the attached schematic?
I can send the password to you by mail.
Thank you.
Schematic.7z
Part Number: TIR1000 My customer would like to study TIR1000 for IR Blaster function implementation.
Currently their product is using TV remote (consumer IR) while TIR1000 states that only compatible for IrDA and HPSIR.
Customer would like to know whether…
Part Number: TIR1000 Dear Team,
From the spec, it seems like we need to provide 1.843MHz clock signal to 16XCLK, but I am not sure if this clock signal is synchronous or not.
Does the clock need to synchronize with internal UART clock of the host(CPU…
Part Number: TIR1000
Dear Team,
Could you please help to check whether there is any concern if we connect the TFBS4652 IrDA SIR module (as attached data sheet shown) to TIR1000's IR_RXD/IR_TXD port directly?
Vishay tfbs4652.pdf
Thank you.
Jim
…
Part Number: TIR1000 Hi team,
My customer wants to know the TIR1000 minimum RESET pulse width. I could not find the value in the datasheet.
Please let me know.
Best regards, Fumio Nakano
Part Number: TIR1000 Dear Sir,
Our customer using Texas instruments IC TIR1000 for IrDA communication process .
Issue :
Receiving same transmitted (echo) data at transmission time.
Please can you suggest how can we solve it on priority.
IRDA Part from…
Part Number: TIR1000 The decoder function on the TIR1000 chip isn't working for us. When we send a signal (to IR_RXD) we don't get anything out on U_RXD (the output stays constant at 3.3 V), based on oscilloscope testing. We have tried resetting and we…
Other Parts Discussed in Thread: TIR1000 Hi,
When operating with TIR1000 datasheet (SLLS228G) Icc has MAX-value written as 1mA.
1. When RESET is set to High, please tell me the consumption current value of Icc. 2. Does it become disabled by setting the…