Other Parts Discussed in Thread: TL026 hi,
my customer uses the TL026C with differencial output and input to GND with +/-6V.
the output is connected to two serial cap of 150nF and with 2 K load.
the output is pretty noisy, could you explainit?
i have…
Other Parts Discussed in Thread: TL026 , LM2611 , LMR70503 I'm looking at using the TL026 in a single-supply application. As far as I can tell, the part really only requires mid-point reference for input biasing; output coupling is AC, and the AGC input…
Other Parts Discussed in Thread: TL026 Can I use TL026 as an input amplification stage for a 10-bit ADC and use PWM with RC filter to generate the gain control signal? Thanks.
Other Parts Discussed in Thread: TL026 [:D]hola buenas tardes, he tratado de implementar el circuito descrito en el datasheet de este dispositivo pero lo unico que consigo es que la señal se mantenga en 1 V, pero la ganancia no se atenua, A amplitudes…
Other Parts Discussed in Thread: TL026 HI all,
I am currently doing a DDS function generator which will generate 20 Vpp sine wave within 0-40 MHz.As frequency higher,the amplitude from DDS module become lower which are when frequency is 1MHz, amplitude…