Hi Meng,
open the TI site of the chip of interest and click the button "quality & packaging". Then find the stastical data in the rightmost column.
Example:
www.ti.com/.../TL052
www.ti.com/.../pinout-quality
www.ti.com/.../estimator…
Hi Tim,
I would add a precision single wave rectifier to the input of OPA541 as shown below. This would allow you to generate a true unipolar signal at the Helmholtz coil without having to adjust the offset voltage whenever you change the amplitude at…
Hi Pavithra,
Please find below the comparison between LM358 and TL052.
LMV358
VccMin:
3 V
VccMax:
32 V
VinMin:
0 from V- rail
VinMax:
-1.5 from V+ rail
VoutMin:
0.005 from V- rail
VoutMax:
-2 from V+ rai…
Hi Mickey,
in the following you see the result of a simplified phase stability analysis for the TL052, as an example. Open loop output impedance is 250R, input capacitance is 12pF. A photo diode with a detector capacitance of 100pF was assumed:
You see…
Part Number: LF412 Other Parts Discussed in Thread: TL052 , TL072 Hi All,
can anyone please let me know what is the max voltage that can be applied to the inputs of LF412 ? i see that the min voltage that can be applied is VEE.
also are there any clamp…
Other Parts Discussed in Thread: TL052 , TINA-TI Hi
I was looking for a high-speed transimpedence amplifier for photodiode sensing appliction. I need a closed loop bandwidth (f-3dB) of at least 1 MHz and an output swing of around +- 5V. The photodiode I…
Hithesh,
The JFET input opamps, like the TL032, TL052, TL072, TL082 have a common mode range up to VCC+. Each one has a different ICC and speed. They are also inexpensive.
Regards, Ron M.