Part Number: TL081H Other Parts Discussed in Thread: TL071H , , TL084H , TL082H , TL074H , TL072H
What's the major difference between TL081H and TL071H? I'm wired about these two family.
Regards
Brian W
The 3.5 mA value is consistent with figure 6 in the datasheet. And even a redesign would not change power consumption and speed by that amount.
5 mA sounds as if it could be something like the LM318. Can you check if there are clamping diodes between…
Part Number: LM4040 Other Parts Discussed in Thread: TL432 , , REF35
Hello TI,
I want to design an accurate small adjustable reference voltage from 100mV to 2.5V.This reference voltage is used to shift-up a measured voltage signal to adapt it to the ADC…
Part Number: OPA602 Other Parts Discussed in Thread: LM6142 , TL071 Hi Team,
Good day. I am posting this inquiry on behalf of the customer.
"I am looking for a replacement for OPA602AP.
I would also only like through-hole parts, no soldering is r…