Part Number: TL1431-SP Hello,
Can you confirm that the NC pins on this device are truly not connected to the die?
We cannot leave these pins floating. Is there a recommendation for this?
Can we connect them directly to GND? Would we need a resistor to…
Part Number: TL1431-SP According to MIL-STD-883 SEM is not required for planar die. Does this apply to the 5962R9962001VHA? Or is it non-planar and SEM is required?
Thank you in advance for your help
Part Number: TL1431-SP Hi,
Could you please provide CFP-10 (U) package details of TL1431-SP?
Pin functions are given for CDIP (JG) package but I need the same for CFP (U) package.
please provide deatiled information regarding CFP (U) package.
Thanks, …
Part Number: TL1431-SP Other Parts Discussed in Thread: TL1431 Hi Support,
Please advise SEE report.
SET: what is the effect on output voltage (delta-V and duration) at various LET doses? Is the component immune to SEL and SEGR?
Thanks.
Part Number: TL1431-SP Other Parts Discussed in Thread: TL1431 , TL431 Do we have detailed data showing reference voltage vs bias current?
Figure 7 of the datasheet provided some guidance for low Ibias levels. We'd like to see a full table up to 10mA with…
Part Number: TL1431-SP Other Parts Discussed in Thread: TL1431 Hello,
I am using the spatial QML-V version of the TL1431 and I would like to know why there is a difference between the TI datasheet (SLVSB44B) which specifies a Vi(ref) between 2.475V and…
Other Parts Discussed in Thread: TL1431 Hello,
I am working on space project and I am looking for any SEE data (especially for Single Event Transient) for the space or military TL1431 version (LETth(SET), shape of the SET,...).
Best regards,
Nicolas …
Part Number: TPS7A4501-SP Other Parts Discussed in Thread: LM117 , TL1431 , We previously used an LM117 to regulate a -200 vdc supply by elevating the potentials on the input and output. The idea was taken from a TI application note. We are trying to get…
Hi Kevin,
For rad-hard 2.5V references, there are a few options: t he LM136A-2.5QML-SP , the 2.5V option of the LM4050QML-SP , and the TL1431-SP . All of these parts do have TID reports (sometimes referred to as ELDRS reports for older documents) available…