Part Number: TL1431M Tool/software: Hello, can you confirm that 5962-9962001Q2A & 5962-87659022A are both available with no planned obsolescence? Mouser shows both as obsolete.
Part Number: TL1431M Tool/software: Hello,
Is the mask for a TL1431MJGB with DC1933 of the the revision B ? (the same as DC1648)
Thanks in advance !
Best regards
Part Number: TL1431M Dear Support,
I'm quite surprised with the min and max reference input voltage stated in our datasheet page 7:
At 25°C, we are qualified at 2.475Vmin and 2.540Vmax, while the other grades (standard, automotive, EP, etc...),…
Other Parts Discussed in Thread: SN54AHC123A , SN54AHC14 , TL1431M , TLC2543M I'm looking for single event effects data for any of the following part numbers: CD4516BF, TL1431M, SN54AHC123A, TLC2543M, SN54AHC14. Any idea of where I can find information…
All these devices were discontinued.
For the TL431M, the replacement is the TL 1 431M: ti.com/product/TL1431M
For the National Semiconductor devices, the replacement is the corresponding device acquired from RCA, e.g., CD4013BMx → CD4013B-MIL. ti…
Hey Lee,
There is a TL1431M which is available in a CDIP package: https://www.ti.com/product/TL1431M Its not full commercial, but its not space grade
Figure 7-2 in the TL1431-SP datasheet shows how you would use the TL1431-SP as a 3.3 V reference…
Part Number: TL1431 Hello!
I would like to use the TL1431 as a window comparator as depicted in Figure 34. Voltage Monitor of TL1431, TL1431M SLVS062N datasheet.
The main issue is the voltage that I should monitor. It is a +270Vdc. Any suggestion…