Other Parts Discussed in Thread: TL16C554A Hi,
I have a question about asynchronous-communication element TL16C554A.
In datasheet(SLLS509E) page.8 "recommended operating conditions, standard voltage(5 V-nominal)" , High-level input voltage VIH…
Other Parts Discussed in Thread: TL16C554A I want to use the TL16C554A to replace the ST16C554, but encounter some problem after populated the TL16C554A, please let me know what should I do now.
Hi Eric-san
Thank you for your quick reply.
I understood.
There is one more question, I would like to ask you regarding this device and TL16C554A.
If RTS*, CTS*,DTR*,DSR*,DCD*,RI* pin aren't used, can these pins left open?
If not, what should I do? …
Hello Stephan,
I apologize for the delay in responding. The only changes from the TL16C554 to the TL16C554A are the 3.3V operation support and the addition of the Autoflow (AFE) capability. The TL16C554A has the same pinout and can be used as a drop…
Part Number: TL16C754C Other Parts Discussed in Thread: TL16C554A , DS36954 , SN74CBT16214 Hi,
Is there any example reference design or schematic available for TL16C754C? (like it is the case with many other components)?
Thanks & regards,
Gunther
Part Number: TL16C754C Other Parts Discussed in Thread: TL16C554A Hi team,
It is nice to know you here. My customer is evaluating TL16C754C. And they met below issue,
The TX data can be received by PC;
When PC sending data to this device, such as "11…
Hey Shashi,
"Does the TL16C554A have any such similar or other problems for baud rate / parity / data & stop bits combinations ?"
This is a bit of a tricky question for us. I do not know the older device's history.
My understanding…
Hello Ben,
The TL16C554A does not need any driver, you only have to set the internal registers to the desired configuration and that's it. Maybe the software you are using is not able to address the internal registers of the TL16C554A on the 64 bits…
Hello Parth,
I received the IBIS model today. I have attached it to this reply. I am working to get it posted to the TI TL16C554A product folder.
Thank you.
Best Regards,
Joe
Wenbo,
The following UART devices all provide the DCD, CTS, DSR, RI, TXD, RTS, DTR, and RXD signals that are required for your application:
TL16C554A TL16C2552 TL16C752C, TL16C754C, TL16C2752C - these all share a common stop bit errata that is being fixed…